Part Number: LAUNCHCC3235MOD Other Parts Discussed in Thread: CC3235SF Hello Team,
I am working with CC3235SF's ADC and GPIO modules. I am using the ADC channels 1,2 and 3 which uses GPIO3(pin 58), GPIO4(pin 59) and GPIO5(pin 60) respectively.
I have…
Part Number: LAUNCHCC3235MOD Other Parts Discussed in Thread: TEST
Hello,
In CC3235MOD datasheet, it is mentioned TCP throughput is 13Mbps. Which example or test code can be used to test the throughput on the LAUNCHCC3235MOD board?
Part Number: LAUNCHCC3235MOD Other Parts Discussed in Thread: UNIFLASH , SYSCONFIG , CC3235SF Hi,
I'm just getting started with CC3235MOD Launchpad Kit. I'm trying to walk through the QuickStartGuide for SimpleLink CC32xxSDK.
My development environment…
Part Number: LAUNCHCC3235MOD Other Parts Discussed in Thread: TEST Hi,
Can you tell me why the out of box program does not see 5Ghz networks.
I am on the settings.html page in "Add profile" / "SSID" the 5Ghz networks are not visible. …
Part Number: LAUNCHCC3235MOD Hello.
If you look at the following document, you will see "Host Application" in the basic architecture. (see www.ti.com/.../swru534)
Is this Host Application similar to the MSP432E401 implemented in the CC3235 Module…
Part Number: LAUNCHCC3235MOD Hello Team,
I am fairly new to TSL/SSL and pardon me if this is a very basic doubt but I am trying to connect to cloud using Websocket headers . The flow for connection as implemented on ESP32 with mbedtls library (as per…
Other Parts Discussed in Thread: LAUNCHCC3235MOD , CC3235SF , SYSBIOS Hello,
I am using the LAUNCHCC3235MOD launchpad. When I am trying to build the hello example projects I get the following errors for both projects.
CCS Version: 10.4.0.00006
**** Build…
Part Number: LAUNCHCC3235MOD Other Parts Discussed in Thread: CC3235SF I am trying to work in CC3235SF on CCS10.
How to connect to google cloud and port certificat file?
Part Number: LAUNCHCC3235MOD Other Parts Discussed in Thread: CC3235SF , CC3235MODSF , TMDSEMU110-U , CC3235S , CC3235MODS Hello,
we had the CC3235SF-LaunchPad and was able to develop the application framework (based on http server example).
things worked…
Part Number: LAUNCHCC3235MOD Other Parts Discussed in Thread: CC3235MODSF , CC3235SF PART NO - LAUNCHCC3235MOD CCS software version - 10.3.1.00003 Jumper are placed in default settings as per the CC3235MODSF SimpleLinkTm Wi-Fi® and IoTSolution With MCU LaunchPadTm…