Part Number: LAUNCHXL-CC1310 Hi Team,
It is possible to use LAUNCHXL-CC1310 at 433 mhz? Can we use SMA antenna and 433 matching circuit? Can you give referance matching circiut for 433 Mhz?
BR, Stefan
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 ,
I have a CC1310 and I'm struggling to get my device to talk to it when running debug in Code Composer Studio but my device talks to it when running SmartRF Studio. I am running project…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310
Greetings
I am looking to configure a GPIO pin, to be set (go "high) in the mainThread. However, when toggling the pin to go "high", it sits at 0V, when I measure the pin's voltage. I…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: SYSCONFIG , CC1310 Greetings
I am trying to configure a CC1310 Launchpad on Sysconfig. My aim is to set the device up for SPI and UART. I am unable to generate the board.c and board.h files but…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 Hi Experts,
I'm able to make software for the CC1310 using CCS and the ccfg.c file so it can be flashed using the CCS or the bootloader using the uart,
I've discovered that openocd…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 , , CC1101 I’m having trouble getting the CC1310 to operate in packet mode at 2.4kbps.
If I take two Launchxl-cc1310 eval boards, and program one with your reference rfEchoTx and…
Part Number: LAUNCHXL-CC1310 After the upgrade does not restart me about what problem based on IAR compiled SDK to simplelink _ cc13x0 _ sdk _ 4 _ 20 _ 02 _ 07
Part Number: LAUNCHXL-CC1310 Hi Team,
Example: Simplelink_cc13x0_SDK_4_20_02_07
Issue: when running, both CCS and IAR are stuck at RF_runCmd().
Could you help check this case? Thanks.
Best Regards,
Cherry
Part Number: LAUNCHXL-CC1310 Hi Team,
Does anybody has 3d step for this board, or at least positions of header and all dimensions?
Thank you
Regards, Serhii
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: WMBUS
Hi Team,
As shown below, the copied routine can be compiled directly without errors.
After rename, an additional directory STWCC13xx_RTOS_Lib_Use will appear, and an error will be reported…