Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: UNIFLASH , , CC1310 , WMBUS , CC1350 Hi!
I'm trying to flash a launchxl-cc1312r1 with "Serial_CC13xx_Collector_T2.hex", so I can communicate with the device via the SATP API Interface.…
Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: UNIFLASH Hi,
I mistakenly programmed my Launchpad with CC1312R1 and locked the Debug options.
I cannot access the device besides trying to Mass erase it, but although the mass erase seem…
Part Number: LAUNCHXL-CC1312R1 Hello,
I have two launchxl-cc1312r1 and try to download example tx and rx (project0) use CCS cloud ( dev.ti.com/.../node .
I have installed ti browser extension and ti cloud agent. But I get error for each module
1st…
Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: SYSCONFIG Hi team,
May I ask you questions regarding manchester coded binary modulation?
1. My customer would like to set the protocol to manchester coded binary modulation(FSK/GFSK)…
Part Number: LAUNCHXL-CC1312R1 Tool/software: 1. The 15.4 protocol stack we use, the RF parameters are generated according to the studio software, and the transmit power is 13dBm.
2. In the previous test, in the open distance, the RSSI can be measured…
Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: WMBUS , , SYSCONFIG , CC1312R Hello, I want to develop WMbus communication using LAUNCHXL-CC1312R1 and a smartmeter that use 433MHz. but there is no WMBus option in sysCfg when I select 420…
Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: WMBUS , SYSCONFIG Tool/software: I want to receive data from WMBUS 433 (434.475MHz) on CC1312R1.
Data sender have this configuration:
freq: 434.475 MHz
symbol rate: 100 kB
deviation…
Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: CC1312R
The head engineer purchased a couple LAUNCHPAD-1312R test boards, to potentially use that MCU/Wireless as a replacement for an EOL narrow-band product we manufacture.
For backward…
Part Number: LAUNCHXL-CC1312R1 Hi,
I am new in CC13xx. I do import from example rRfPacketRx. And I am trying to print rx packet thru UART.
But, No UART element in syscfg window. Only UART2. I attached capture image.
What is the problem?
BR…
Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: LP-CC1312R7 Hi
I'm looking for an IC that covers the 400MHz, 900MHz, and 1200MHz bands.
I am currently adjusting the 1200MHz band using CC1312R1, and although it says that it is supported…