Part Number: LAUNCHXL-CC1350 Other Parts Discussed in Thread: CC1350
Hello there,
I am running rfPacketTx on the CC1350 launchpad and it works fine if I source 3.3V through the header pins (switching to the external power jumper). How do I make it work…
Part Number: LAUNCHXL-CC1350 .txpower value is set to 0xAB3F in rfPacketTx code for the transmission power of 14 dBm. I have to transmit the packets at 0 dBm. Is there any lookup table between the .txpower value and dBm?
Part Number: LAUNCHXL-CC1350 Other Parts Discussed in Thread: UNIFLASH Hi Team,
Could you help our customer for their concern below.
I have a LAUNCHXL-CC1350 eval board. When I connect the device to the computer via USB, I cannot see the Bluetooth name…
Part Number: LAUNCHXL-CC1350-4 Other Parts Discussed in Thread: CC1350
Hi all,
I am working with the UART CC1350 chip, and try to using the FIFO TX and Rx.
I searched on the document technical user guide and found the UART FIFO at section 19.1, 19.2, and…
Part Number: LAUNCHXL-CC1350 Other Parts Discussed in Thread: MIOTY , CC1350 , CC1310 I am using CC1350 Launchpad for my project along with Stackforce MIOTY stack API evaluvation for CC13x0 devices. But I am unable to add device in the MIOTY gateway. On…
Hi Marie H
Thanks for the reply, i have changed to Legacy Long Range mode the communication has good range but i can't achieve the distance in Energia with EasyLink library,
In 43oh.com forums for Energia support . no one is answering for CC1350,
else…
Part Number: LAUNCHXL-CC1350-4 Other Parts Discussed in Thread: CC1350 Hi all.
I have two CC1350 launchpad and use CCS studio to make a RF bridge between them.
RF setting by SMART RF studio at 915Mhz, 0dbm output power.
When using Smart RF studio panel…
Part Number: LAUNCHXL-CC1350-4 Hello, I am having 2 very serious issues with the CCS environment.
On Windows, I am unable to use the resource explorer at all. If I make a new workspace I get a few seconds of seeing things, then it goes blank. Attempting…
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: C2000WARE-MOTORCONTROL-SDK , C2000WARE Hello,
We would like to use at our company this prototype inverter " 200kW Three-Phase Inverter with XM3 Power Module | Wolfspeed ", but since it is…
Part Number: LAUNCHXL-CC1350 Other Parts Discussed in Thread: CC1350 , CC1000 Hello, We have a 434MHz wireless temperature sensor and the data is transmitted with a CRC-8 data verification.
With The LAUNCHXL-CC1350 we can receive the sensors and see it…