Part Number: LAUNCHXL-CC1350-4 Hello, I am having 2 very serious issues with the CCS environment.
On Windows, I am unable to use the resource explorer at all. If I make a new workspace I get a few seconds of seeing things, then it goes blank. Attempting…
Part Number: LAUNCHXL-F280025C I am using the LaunchXL-F280025C with the BoostXL8323RH.
I am trying to use Build 4 of the Motor Control Lab with a motor where I do not have a lot of the parameters.
When the the EST switches from EST_STATE_CONSTSPEED to…
Part Number: LAUNCHXL-CC1350 Hi team,
Here's the request from the customer:
Customer found that UART is the MODE of FULL, and many resources are written Uart (uart, &input, 1), which can only read one word at a time. If it is possible to dynamically…
Part Number: LAUNCHXL-CC1350 Other Parts Discussed in Thread: CC1350
Hello there,
I am running rfPacketTx on the CC1350 launchpad and it works fine if I source 3.3V through the header pins (switching to the external power jumper). How do I make it work…
Part Number: LAUNCHXL-CC1350 .txpower value is set to 0xAB3F in rfPacketTx code for the transmission power of 14 dBm. I have to transmit the packets at 0 dBm. Is there any lookup table between the .txpower value and dBm?
Part Number: LAUNCHXL-CC1350-4 Other Parts Discussed in Thread: CC1350 Hello TI community,
I am working with cc1350 and my application involves use of multi-tasking (threads/interrupts/timers) in Code Composer (in particular, run adcbufcontinuous example…
Part Number: LAUNCHXL-CC1350-4 Other Parts Discussed in Thread: CC1101 , CC1350 , CC1200 Hi,
Can I use the 802.15.4g FEC in LAUNCHXL-CC1350-4?
I find this from datasheet, but I didn't find any option about 802.15.4g FEC in SmartRF Studio.
tks.
Part Number: LAUNCHXL-CC1350 Other Parts Discussed in Thread: MIOTY , CC1350 , CC1310 I am using CC1350 Launchpad for my project along with Stackforce MIOTY stack API evaluvation for CC13x0 devices. But I am unable to add device in the MIOTY gateway. On…
Part Number: LAUNCHXL-CC1350 Other Parts Discussed in Thread: UNIFLASH Hi Team,
Could you help our customer for their concern below.
I have a LAUNCHXL-CC1350 eval board. When I connect the device to the computer via USB, I cannot see the Bluetooth name…