Hi,
This will be released separately from the SDK, so I expect it to go live on the app stores in a couple of weeks. I will try to see if I can provide a better estimate.
Best Regards,
Jan
Part Number: LAUNCHXL-CC26X2R1 Other Parts Discussed in Thread: UNIFLASH Hi,
I am using SDKv7.10 and Uniflash 8.1.1. What load address should I set it to?
-kel
Part Number: LAUNCHXL-CC26X2R1 Hello,
when we connect mobile application to the Bluetooth then Some mobile devices are suddenly unpaired or not allow to connect. can you please help me to solve this problem. Is issue related to MITM or any other parameter…
Part Number: LAUNCHXL-CC26X2R1 Other Parts Discussed in Thread: SYSCONFIG Hi all,
I am back at CC26x2r after a while
I have a quick question, well, 4 small ones, since sometimes it takes a lot of attemps to connect my cc26x2r to a linux raspberry system…
Part Number: LAUNCHXL-CC26X2R1 Other Parts Discussed in Thread: BLE-STACK Hi Ti teams:
This is the map file. And the heap size is 6655 Bytes.
When I download this fireware and it is failed to start.
Then I change setting to set the heap size to 34303…
Part Number: LAUNCHXL-CC26X2R1 Other Parts Discussed in Thread: SYSCONFIG
Is there a way to add conditional statements in syscfg file?
Something like:
#if defined DEBUG
XYZ.addr = 0x1000
#else
XYZ.addr = 0x5000
#endif
Part Number: LAUNCHXL-CC26X2R1 Dear,
I downloaded the app for my iphone 12.
I can see all the features, looks nice.
However, when trying to upload one image generated by me, I go to OAD enhanced / select FW file, scroll down to "uploaded images" since…
Part Number: LAUNCHXL-CC26X2R1 Other Parts Discussed in Thread: CC2642R-Q1 I am trying to flash CC2642R-Q1 in Backdoor boot loader mode via SPI.
After reset, the chip is responding to PING command after 5s. Is that expected?
And if i continuously send…
Part Number: LAUNCHXL-CC26X2R1 Other Parts Discussed in Thread: CC2541 , ENERGYTRACE We were looking to reuse the BLE CO sessor
https://www.digikey.com/en/products/detail/texas-instruments/GASSENSOREVM/4764883
And while we found code and everything we…
Part Number: LAUNCHXL-CC26X2R1 How can read RSSI value?
I have a board(CC2652R1),t hen I used the simple_peripheral_CC26X2R1_LAUNCHXL_tirtos7_ticlang SDK.
My cc2652 is for the broadcaster and now I need to get the RSSI without making a connection.How to…