Part Number: LAUNCHXL-CC3235S hello everyone
I have a bunch of processed numerical data that I want to store on a USB flash stick, connected to the CS3235s usb port.
I wonder if it is possible, and yes, is there any library/sample code available online…
Part Number: LAUNCHXL-CC3235SF Hi TI engineer
I want to get avaliable heap size to limit heap use when system running. Is there hava function to get avaliable heap size?
Part Number: LAUNCHXL-CC3235S Other Parts Discussed in Thread: CC3235S Hi
i have the CC3235S launchpad, the sole onboard profile is created when i perform the provisioning/configuration via the TI iPhone SimpleLink app.
The CC3235 then auto connects to…
Part Number: LAUNCHXL-CC3235S Other Parts Discussed in Thread: CC3235S , CC3235SF Hello everyone,
I am looking for OpenSSL library, compatible with CC3235s. It seems the official OpenSSL libary is not compatible with the board.
Wondering if there is any…
Part Number: LAUNCHXL-CC3235S Other Parts Discussed in Thread: CC3235S , SYSCONFIG I'm trying to run the network_terminal sample on my LP-CC3235S, but when I compile the program, I get the errors below. I'm using CCS 12.3.0.00005, but have also tried…
Part Number: LAUNCHXL-CC3235S Other Parts Discussed in Thread: UNIFLASH , CC3235SF , SYSCONFIG , CC3235S Hi
i'm using the lauunchxl-cc3235 to connect to a modified version of the TI concentrator program to my app thats on a win10 pc.
CCS i'm using is…
hello Shlomi,
Shlomi Itzhak said: Do you mean a way to control the Wi-Fi MCS rates (like MCS0-MCS7)?
Yes, I meant exactly the same.
Shlomi Itzhak said: If this is the case, there is no way to control it since it is automatically set as part of the rate…
Part Number: LAUNCHXL-CC3235S Hi TI team,
I'm developing an application that creates an AP using CC3235, configures the AP parameters, waits for STA to get connected, creates a socket and start data transmission to STA.
While the system is in action…
Part Number: LAUNCHXL-CC3235S Other Parts Discussed in Thread: CC3235S , SYSCONFIG
Hi
[edit] this has been resolved...the COM jumpers for Rx & Tx i had set for using the headers and not the USB com....
I'm trying to build my previously working program…
Part Number: LAUNCHXL-CC3235SF According to swra510b.pdf Application Report TI WiFi chip supports OTA file transfer using Dropbox and Github Cloud support only.
According to TI source files OTA could support firmware update over HTTP.
Could you provide…