Part Number: LAUNCHXL-F280049C Other Parts Discussed in Thread: BOOSTXL-DRV8320RS , C2000WARE-MOTORCONTROL-SDK , C2000WARE Hello
I have purchased BOOSTXL-DRV8323RX with LAUNCHXL-F280049C for Evaluating InstaSPIN FOC for running a motor at 90,000 rpm.
On…
Part Number: LAUNCHXL-F280049C Other Parts Discussed in Thread: SYSCONFIG Hello, I want to use LAUNCHXL-F280049C for testing my board. I need total of 16 PWM signals as output but in the documentation it was mentioned that only 14 PWM signals are possible…
Part Number: LAUNCHXL-F280049C I want to generate analog three-phase AC voltage with LAUNCHXL-F280049C.
However, only two analog voltage can be generated from LAUNCHXL-F280049C.
That's why I bought two LAUNCHXL-F280049C.
Therefore I wanna synchronize…
Part Number: LAUNCHXL-F280049C I want to generate analog three-phase AC voltage with LAUNCHXL-F280049C.
However, only two analog voltage can be generated from LAUNCHXL-F280049C.
That's why I bought two LAUNCHXL-F280049C.
Therefore I wanna synchronize…
Part Number: LAUNCHXL-F280049C Other Parts Discussed in Thread: C2000WARE , SYSCONFIG Hi,
I am trying to generate a single double-pulse signal for driving a MOSFET double pulse testing rig using the EPWM module. The goal is to achieve a waveform similar to…
Part Number: LAUNCHXL-F280049C Hi,
I need some clarification on the strange behaviour of my Code.
I just enabed the idiv0 processor support option of the F280049C launch pad and some diviison operation returns 0 while others works well.
Why this strange…
Part Number: LAUNCHXL-F280049C Hi,
I have an application in which I require to
Use one analog signal to generate three different trip events using CMPSS (three different units with different DAC value).
Then use these 3 trip signals to generate the switching…
Part Number: LAUNCHXL-F280049C Hi Team,
There's an issue from the customer need your help:
I encountered the following problems when transferring data:
Data transfer from FLASH to GxRAM is carried out through the memcpy interface of string.h. The…
Hi Shahar,
Shahar Cohen said: Are the settings in the previous image okay for our setup?
It may be better to start with the default settings however. Disable the below and keep others the same.
OVM
FWC
MTPA
SSIPD
VOLRECT
STEP_RP
Best,
Kevin
Part Number: LAUNCHXL-F280049C Other Parts Discussed in Thread: SYSCONFIG
Where can I check the Positive input value of CMPSS 1 in a register? I want to confirm this because I would like to see the sensed value and verify if it reads within the range…