Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: DRV8305 , MOTORWARE Hello sir,
I am using LUNCHXL F28027F + DRV8305 for controlling BLDC Motor. Speed of motor varies from 900 to 8000. But motor doesn't stop immediately. Is there any…
Which example lab/project are you using? Or your own algorithm?
Thomas Hecht said: If the motor is now driven to a stop so that it can not rotate further, the motor makes a knocking noise and jerks (torque increases and then drops again)
Do you have…
Part Number: LAUNCHXL-F28027F Hello, Everyone.
I just wondering, where i should connect the QEP sensor from the motor Teknic 2310P using LaunchpadXL F28027F, i just cant find that pin on the microcontroller board. What the J3 for?
Thanks in advance…
Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: DRV8353 , DRV8353RS-EVM , MOTORWARE We are using ISO-F28027F MCU Board interfaced with DRV8353RS-EVM Board to run the 48V BLDC Motor. We used lab05b code of DRV8353 EVM firmware file for this…
Hi,
Farhan Sumantri said: when im running lab1b im not able to observe the gDacData variable
Is gDacData declared with global scope? It needs to be global to view in expressions window, if that's how you're wanting to view it.
Farhan Sumantri said…
Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: DRV8353 , ISO7740 , C2000WARE-MOTORCONTROL-SDK , DRV8353R , TMDSEMU110-U Hi Experts,
Our customer wants custom LAUNCHXL-F28027F for control DRV8353, but ICs ISO7240 and ISO7232 are out…
Part Number: LAUNCHXL-F28027F I am a beginner using the LAUNCHXL-F28027F. I am looking for a series of easy-to-follow tutorials such as this one for the TivaC series: https://software-dl.ti.com/trainingTTO/trainingTTO_public_sw/GSW-TM4C123G-LaunchPad…
Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: MOTORWARE I am new to the c2000 family and recently tries to utilize the HRPWM module to get Duty cycle of 50.3% at 500KHz switching frequency with the clock seed set to 60MHz. Below is the…
Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: CONTROLSUITE Hello,
Does anyone have sample source code to generate carrier-type PWM signal with the « LAUNCHXL-F28027F ».
Purpose is to generate a Full-bridge signal control for a single…
Part Number: LAUNCHXL-F28027F Other Parts Discussed in Thread: MOTORWARE , DRV8305 , TMS320F28027F I am using motorware lab 02b to build project and then using the output file and renaming it to appProgram in Universal GUI folder.
The target is initialized…