Part Number: LAUNCHXL-F28069M Tool/software: So my current setup is that I have 2 CC2640r2 bluetooth boards and I have successfully connected them over bluetooth and am passing joystick data between the two. The last step I am trying to accomplish is…
Part Number: LAUNCHXL-F28069M
Tool/software:
The USER_ErrorCode_iqFullScaleVoltage_V_Low appears during debug but I cannot fulfil the following conditions:
if((USER_IQ_FULL_SCALE_VOLTAGE_V <= 0.0) ||
(USER_IQ_FULL_SCALE_VOLTAGE_V <= (0.5 * USER_MOTOR_MAX_CURRENT…
Part Number: LAUNCHXL-F28069M Other Parts Discussed in Thread: BOOSTXL-DRV8323RS Hi,
I have experience using the InstaSPIN labs for single motor position control and building custom control loops. My current hardware is a custom PCB based on the LaunchXL…
Part Number: LAUNCHXL-F28069M Tool/software: Here we use DRV8353RH EVM + LAUNCHXL-28069M as motor driver
After excitation, FOC control starts. Tof sensor is disconnected.
From the oscilloscope, there is a noise on CLK before the end.
Is there any…
Part Number: LAUNCHXL-F28069M Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM , C2000WARE , MOTORWARE Tool/software: Hello I am working with a LaunchXL-F28069M board and a BOOSTXL-DRV8305EVM BoosterPack motor driver. Based on my understanding, the…
luca debs said: Do I calculate it? Is it measured?
Mostly, you can find the parameter in the motor datasheet.
luca debs said: IS THIS CORRECT?
Right. You can calculate the Flux based on BEMF constant.
BTW, you may ask the FOC algorithm design…
Part Number: LAUNCHXL-F28069M Other Parts Discussed in Thread: DRV8305
Tool/software:
I am testing lab01b using LAUNCHXL-F28069M and DRV8305.
When I set gMotorVars.Flag_enableSys to 1 it remains 0, I do not understand why.
It almost seems as if…
Part Number: LAUNCHXL-F28069M Other Parts Discussed in Thread: MOTORWARE , TMS320F28069M , BOOSTXL-DRV8301 Tool/software: Hi everyone, I am working on Lab 5C and Lab 12A from the MotorWare motor characterization labs to perform inertia identification…
Part Number: LAUNCHXL-F28069M Tool/software: I am running lab12a interfacing the quadrature encoder for the first time. When I set flag_enableSys and Flag_Run_Identify to one the motor jumps to a position and draws a ton of current and buzzes. I have…