Part Number: LAUNCHXL-F28379D Tool/software: I have worked for some years with LauncherPad 28379D ver:1.2
It always worked fine, but one day with a brand "new" board, my old codes stopped working. After investigation, I saw the "new" board was an older…
Part Number: LAUNCHXL-F28379D Tool/software:
How do I find the project settings that select the _LAUNCHXL_F28379D and hence be able to use the settings defined under this section?
Currently with the example projects that I have imported, I am not…
Part Number: LAUNCHXL-F28379D Tool/software: When I build and try to debug or flash the code, The CCS theia notifies that " No compatible debug core found." What may be the potential reason for not be able to flash and debug the code in CCS for the given…
Part Number: LAUNCHXL-F28379D Tool/software: When I try to debug the code, I am getting the following error : IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation…
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM Tool/software: Good afternoon, I'm working on implementing the ADC module into my project but it is currently reading incorrect values. It works well with non changing voltages…
Part Number: LAUNCHXL-F28379D Tool/software: Hello Forum,
I am using a Launchpad XL to store data from the drone during flight for 1 second. I would like to store the captured data from the sensors into flash and then retrieve it from flash once the…
Part Number: LAUNCHXL-F28379D Tool/software: Hi TI-team,
I would like to ask if DSP28379 is compatible with RTbox2, and if it can be used to implement an LLC resonant converter demo.
Part Number: LAUNCHXL-F28379D Tool/software: Hello, TI staffs,
I would like to realize the VDS voltage sensing and ID current sensing externally for a single power Silicon MOSFET under DC Power Cycling with MCU or FPGA. Currently looking for an existing…
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hi,
I started a new development on LAUNCHXL-F28379D and strangely it seems that the clock is running at half of what is configured and expected. I double checked…
Part Number: LAUNCHXL-F28379D Tool/software: Hi,
I want to develop a interface board for LAUNCHXL-F28379D having ADC input signal conditioning for hall current senor (LA-55p) and PWM level shifter for controlling a three phase Inverter for AC motor…