Part Number: LAUNCHXL-F29H85X Tool/software: Hi Team,
can we add the Rise time delay to both EPWMA and EPWMB in CCS20.
i have requirement which needs to add rise time delay for both the signals.
Ryan Ma said: This will need to go to our ADC expert. Please create a separate thread for this one.
I can help answer these queries. If these help answer your questions please mark this thread as resolved and I can help get the above thread assigned…
Part Number: LAUNCHXL-F29H85X I have question regarding interrupt performance. My setup:
ADC with repeat active (50MHz, 6 ACQPS, n channels with m repeats)
Trigger of the repeater via ePWM1
RTDMA trigger via ADCA interrupt
Due to the memory…
Part Number: LAUNCHXL-F29H85X Tool/software: Could you please confirm SKU LAUNCHXL-F29H85X i s CE and if YES, please provide t he CE/EU Declaration of Conformity (EU DoC)?
We could not find the CE/EU Declaration for this part on your website.
Thank…
Part Number: LAUNCHXL-F29H85X Other Parts Discussed in Thread: SYSCONFIG I am currently working with the mcan_ex6_transmit_syscfg example and have made the following changes to configure it for Classic CAN , so that the transmitted messages can be viewed…
Part Number: F29H850DM Other Parts Discussed in Thread: TPS653860-Q1 , TPS650366-Q1 , F29H85X-SOM-EVM , LAUNCHXL-F29H85X Hi team,
The F29 requires 1.19V minimum for VDD rail, however, this devices does not have a VDD BOR. Customer need to select a external…
Part Number: TMS320F28030 Other Parts Discussed in Thread: LAUNCHXL-F29H85X Tool/software: Hello,
We would like to get access to the LAUNCHXL-F29H85x for some early predevelopment.
Can you please tell me if early engineering samples can be provided…
Hello,
Snambiar said: 1. For the option 1 OAD, are there any bootloader settings I would need to implement on the receiving F28379D LaunchPad.
Yes, you would want to use the SCI bootloader to help achieve option 1. There is example code in C2000Ware…