Part Number: LDC0851 I recently created a small sensor board with a few small racetrack stacked coils (8 turns, 3.5mil traces, 3.5mil spacing, 1 oz copper, 6mm x 3.3mm). Each coil had its own LDC0851 on an accompanying control board.
Two of the coils…
Part Number: LDC0851 Other Parts Discussed in Thread: LDC1101 , TMAG5170 Hi,
I want to use LDC0851 for event counting for paddle wheel systems.The paddle wheel have 5 teeth and rotating about 7000 rpm.
I use pvdf teeth with 316 stainless steel about 1mm…
Part Number: LDC0851 There seems to be an error in the datasheet. The third sentence of 8.1 Overview is conflicting:
"The push/pull output (OUT) switches low when the sense inductance drops below the reference and returns high when the reference inductance…
Part Number: LDC0851 I need the sensor to detect a moving metal chain when it comes in close proximity.
The sensing coil needs to be mounted on metal surface as well. Will this have any effect on the sensing capability?
Part Number: LDC0851 Hi Experts,
LDC0851 uses a PCB coil. Could our customer use an external coil or not? The reason for asking is that the customer needs to make the board smaller and as he see form the datasheet PCB coil is bigger on 2 PCB layer and…
Part Number: LDC0851 Hi Team,
Good day! With the help of our customer, we notice some ambiguity from the datasheet of this device.
In the LDC0851 data sheet "SNOSCZ7A –DECEMBER 2015–REVISED JANUARY 2016" there are two equations that to me seem to contradict…
Part Number: LDC0851 Dear All,
I am working on project of three phase hall effect sensor replace to three LDC0851 IC with three signal output H1,H2 and H3.
The main application is to calculate motor speed. In our case we are using target disk contains…
Part Number: LDC0851 Hi,
I would like to use the WEBENCH Coil Cesigner that accompanies this product. However, when I export the CAD design it appears to be made for Cadence Allegro v 16. At our company we use v17 which is not compatible with v16 with…