Other Parts Discussed in Thread: LDC0851 , LDC0851EVM We are planning to develop a proximity sensor that utilizes the LDC0851. First, we are considering introducing an evaluation module (LDC0851EVM) to see if the LDC0851 can perform the desired proximity…
Part Number: LDC0851 Sorry to rain on your parade, but The proximity sensor we are designing has a response frequency of 5Khz. I would like to know the inductance and capacitor of the sensor when the maximum Q is achieved, considering the parasitic capacitance…
Mr. Mekre
Thank you very much for your answer. I have a basic question: Does the LDC0851EVM assume that there are two sensor coils? In that case, two LDC_COIL_EVM boards are required. In that case, do I need two LDC_COIL_EVM boards? Does it require two LDC_COIL_EVM…
Mr. Mekre
Thank you very much for your answer. This time, I would like to use LDC_COIL_EVM in addition to the prototype coil to evaluate the PCB stacked coil. size capacitor to C-X (A~S) of each board X (A~S)?
In this case, I will be using LDC0851EVM, and…
Part Number: LDC1312 Other Parts Discussed in Thread: LDC0851EVM , , LDC0851 , LDC1314 , LDC1612 , LDC1614 Thank you very much for your help. I am on the verge of designing a proximity sensor using the LDC0851EVM. Please let me know the following.
1. heat resistance…
Part Number: LDC0851 Thank you very much for your help. I would like to connect a 90mm diameter sensor coil to the LDC0851EVM. I would like to connect a 90mm diameter sensor coil to the LDC0851EVM and have it detect an object even if it is a target (mold…
Hi Justin,
I'm sorry that I could only get back to you know.
We unfortunately do not have the necessary tools to measure Rp and we do not have the LDC0851EVM coil.
I have however changed the capacitor to 82pF and measured the following on the Sensor…
Thank you for your help. Table 4 of the LDC0851EVM shows the list of parameters for the LDC0851. What do you mean by Please tell me the meaning of Trace Width, Trace Spacing and Trace Thickness. What do Trace Width, Trace Spacing and Trace Thickness mean…
Part Number: LDC0851 We have made arrangements for LDC0851EVM. We would like to evaluate the EEVM as soon as we get it. Please let us know about the LDC calculation sheet.
d54: din/dout The calculation sheet says d54=d57/d27, but Please tell me how d54 and…
Hello,
HIROAKI YOSHIDA said: Is the procedure to adjust C,M,N,dout,dL,S,W to get the value of EST inductance with target Interaction?
Yes. For a circular inductor, you won't change dL, but everything else can be changed to adjust the inductance.
HIROAKI…