Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 Hi Team,
I want to use the LDC1101EVM via SPI communication. I can communicate with the device, but the data I receive is inaccurate or nonsensical. I want to see the L and RP values …
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 Good morning,
I've been trying to test the LDC1101EVM for a couple of days without any luck. As of right now the board is correctly identified by Windows, as it shows up as EVM in device…
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 , Looking for the native firmware shipped on the LDC1101 EVM. There are two GUIs linked on the EVM page ( www.ti.com/.../LDC1101EVM . The first points to SNOC028F, which is the generic sensing…
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 Hello,
I am experiencing an issue with the LDC1101 EVM and the Sensing Solutions EVM GUI.
The GUI successfully detects and recognizes the LDC1101 EVM module, and the device appears to…
Part Number: LDC1101EVM my sensor parameters are -
Solid copper coil with ferrite core
input current - 10mA
No. of turns - 4000
sensor frequeny - 5kHz
I am currently having LDC1101EVM and I want to replace its sensor pcb coil with the above…
Part Number: LDC1101EVM Tool/software: Hello Team,
One of our customer claimed a board LDC1101EVM due to configuration/ streaming data issues. We sent out replacement but customer issues remains unsolved. Please see the following,
---------------…
Part Number: LDC1101EVM I have ordered this device and test it both with Python and the GUI. First there are several GUI available, one with the National Instruments runtime, which seems to date from 2014, and another one, which look a lot more simple…
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 , , LDC1614EVM I have followed all the instructioons provided in THIS POST . I have installed:
NI VISA driver: NIVISA1401full
Labview runtime: LABVIEW2010 SP1 Runtime - LVRTE2010_SP1f5std…
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101
Tool/software:
Hello,
after installing EMV GUI v1.10.0 and .NET Framework 3.5, I still cannot write registers and don't get a data stream.
The COM-Port is EVM (COM7). The GUI connects…
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 Tool/software: The LDC1101 EVM is connected to the computer, and a COM port appears. However, the name of this COM port in the Device Manager is not "EVM (COM)" but a Chinese name (see the…