Part Number: LDC1101EVM Hi,
Our customer installed the following tools and connected the LDC1101EVM to the PC's USB port.
・ SensingSolutionsGUI-1.10.0-windows-installer.exe
・ Python_Firmware_Upgrader
However, starting "Data Streaming" does not start…
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1614 ,
Hello,
I'm reading Q3 and Q4 of the inductive sensing FAQ , and I'm not sure where in the LDC1614 documentation it discusses CRC-8 or how to format the " Write register command header…
Hello Bill,
I would start by checking that the data buffer is completely clear after you stop the streaming. This way when you run the streaming again, there isn't any data from the previous run left.
Best Regards, Justin Beigel
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 Hello, I'm trying to communicate to LDC1101 EVM throuth a serial terminal softwae on my PC. The EVM Users Guide mentioned how to use the communication protocal.Then let me confirm. In the…
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 The LDC1101EVM eval board allows the user to configure the voltage supply for the LDC1101, either 1.8V (default) or 2.5V. The datasheet specs the LDC1101 at Vdd=1.8V, and states that the…
Part Number: LDC1101EVM I have a problem with my LDC1101EVM. From the beginning I could not connect the GUI to the COM port. Then I connected R12 to C14. After that, the red LED stopped shining. It seems that the MCU won't start after I power it up.…
Part Number: LDC1101EVM Hello, just received the LDC1101EVM board and installed the GUI. The board is listed in Device Manager as "EVM (COM8)", but in the GUI the COM Port pulldown is blank so the evm does not connect. I am using a Windows 10 PC.…
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 , Hi,
I have an LDC1101 EVM and it was working fine with the LDC1101 EVM GUI, however I updated the firmware with the Sensing Solutions GUI.
Since the firmware upgrade it no longer works…
Part Number: LDC1101EVM
Hello,
I am having issues trying to get the EVM GUI working. I tried installing the setup.exe as an admin and running the EVM GUI in Windows 7 compatibility mode.
I am using a computer that is running Windows 11. I am stuck that…
Part Number: LDC1101EVM Other Parts Discussed in Thread: LDC1101 Hello everyone,
As told by Justin, I followed steps to find out Rp and L values through MATLAB coding.
I am using the "0620" command to start streaming data and gathering data afterward.…