Part Number: LDC1312EVM Other Parts Discussed in Thread: LDC1101EVM , LDC1312 Hello,
Recently, I purchased some Inductive sensor EVMs(LDC1312EVM, LDC3114EVM, LDC1101EVM) from TI store
Every EVMs works well except LDC1312EVM.
LED was ON when I plugged…
Part Number: LDC1312EVM Other Parts Discussed in Thread: LDCCOILEVM , LDC1312 We have purchased the LDC1312EVM and set it up so one of the channels is connected to a LDCCOILEVM example coil. The coil chosen is coil C (100 x 8mm, 17 turns, 4mil trace, 4mil…
Part Number: LDC1312EVM Other Parts Discussed in Thread: LDC1312 I have been using the LDC1312 until i did a firmware update.
The board is now not recognised when connected and has no LED lit.
I followed the [FAQ] My Inductive Sensing EVM won't connect…
Part Number: LDC1312EVM Hi,
I installed the sensing solutions app for use with the LDC1312EVM, but the app only opens to a blank screen. During the install process, the driver installation did not occur as indicated in the user guide (snou135a). The…
Part Number: LDC1312EVM Hello,
We are using the LDC1312EVM and having difficulty getting consistent data from the GUI when we repeat tests at a later time.
Maybe it has to do with the auto calculated Total Inductance parameter, but I’m not sure how that…
Part Number: LDC1312EVM Hi,
my customer evaluates the LDC1312EVM Rev. A. He uses the GUI that detected the EVM right away. Since the sensor didnt output any values, he tried a FW update of the board via the GUI. Now the laptop doesnt detect the EVM anymore…
Part Number: LDC1312EVM After updating EVM Firmware to the version, which is delivered with the EVM GUI-1.10.0, EVM board will not detected from the Computer .->> "unhnown USB device".
I used for updating the "MSP430 USB Firmware upgrade…
Part Number: LDC1312EVM Tool/software: TI C/C++ Compiler
As shown in Figure 1, I don't know why my LDC 1312 board recognized HDC after the connection was successful.
When I upgraded the firmware, the download interface was stuck. Is there any solution…
Part Number: LDC1312EVM Other Parts Discussed in Thread: LDC1312 Tool/software: TI C/C++ Compiler
As shown in Figure 1, I don't know why my LDC 1312 board recognized HDC after the connection was successful.
When I upgraded the firmware, the download…
Part Number: LDC1312EVM Other Parts Discussed in Thread: LDC1314 , LDC1312 , I've set up a linux serial port to talk to the 1312EVM. I send a reset command and then set the registers to
0x1a 0x0201
0x1b 0x8209
0x14 0x110a
0x15 0x110a
0x08 0x0006
0x…