Part Number: LDC1312EVM Other Parts Discussed in Thread: LDC1312 Tool/software: Linux I'm trying to talk to the EVM via a terminal. I did get minicom to connect and once I got a response from the MSP430, but I have no idea what I actually sent to get…
Part Number: LDC1312 Hi,
I am using the LDC1312 Eval Board and Eval Coils (B+C).
The coils, once past concept, will be used in metal tubing.
Can the coils be adjusted to not react the the metal tubing and only to the magnet?
Eval Board - LDC1312EVM Evaluation…
Part Number: LDC1312EVM Other Parts Discussed in Thread: LDC1312 , Hello Eveyone,
I'm using the LDC1312 EVM to designing a new kind of Inductive Sensor. I have my own coil with L = 2260 uH and the capacitor to create the tank circuit is C = 3,3nF. The…
That's nicely done - not complicated!
Now for a 'Agh-h-h!' :-)
I don't know how - the two were right next to each other - but I just noticed that 'writeReg()' got missed in my copy-pasting...
void writeReg(byte bADDR, byte bREG…
Part Number: LDC1312EVM Other Parts Discussed in Thread: LDC1312 , Hi ~ Ti team
I had installed " ldc1312 driver" from C:\ti\Sensing Solutions EVM GUI-1.9.2\EVM Driver to Ldc1312-evm , and it had been working .
when I update "LDC1312_fmwr_07.txt…
Part Number: LDC1312EVM Hi Inductive Sensing Team,
One of my customers and me are having trouble with the LDC1312EVM; the device is not reporting inductance/frequency measurements on the Sensing Solutions GUI, only raw code. We tried flashing with the…
Part Number: LDC1312EVM Hello
I ordered one of the LDC1312EVM board through Digi-Key and realized, but too late, that they sent me a RevA, not RevB.
I unfortunately flashed the RevB firmware using the Sensing Solution UI tool and now it comes back as…
Part Number: LDC1312EVM Hi Team, I would like to ask about LDC1312EVM. I couldn't set "Fin Select" more than 2 in Sensing Solutions EVM GUI. Why it can't be set? I believe CH0_FIN_DIVIDER has 4bit long(0x14[15:12]). Best Regards, Yaita / Japan…
Part Number: LDC1312EVM
Hi Team, There is external 40-MHz oscillator on LDC1312EVM. Should we divide more than 2 if using single channel operation because of the following Table 1? I would like to ask what is concern if we use fREFx=40MHz when single channel…
Other Parts Discussed in Thread: LDC1312EVM , LDC1312 Hello,
We started working on LDC1312EVM with 14mm coil and we could see the change in code however we were not able to see the change in inductance value
So could you please help me on this.
We later…