Part Number: LDC1612 Hi,
In my design I am using LDC1612QDNTTQ1 part, Can you please support on Rectangular coil design calculation ? and also suggest which one, circular or rectangular coil shape is good ? for more range detection. I am using 4 layer PCB…
Other Parts Discussed in Thread: LDC1612 Hai all,
I am currently working on inductive sensors for longer sensing range and I came across LDC1612/1614 as a solution for the same.
But, while going through the datasheet I have a few queries:
1) what is the…
Part Number: LDC1612 I have done a very simple sensor design with the LDC1612 using both channels and am seeing much higher current consumption than the data sheet would suggest. The part is drawing about 20mA of current. According to the data sheet,…
Part Number: LDC1612
Hi Ti, I'm testing LDC1612 and now I found a problem, when the target is in steady state, the output data of LDC1612 is not a straight line. I want to know why and how to improve my design.Help me please~~~
L:Ferrite Magnetic…
Part Number: LDC1612 Other Parts Discussed in Thread: LDCCOILEVM , Hello,
I am utilizing a LDC1612 with a F28379D launchpad to measure lateral movement on coil B from the LDCCOILEVM. Yesterday, I was able to create a 1mm resolution scale used from LDC…
Part Number: LDC1612 Other Parts Discussed in Thread: LDC1614 What’s the maximum distance that the sensor will reliably work from.
Will the sensor detect a bolt through plastic (in addition to its own housing).
What’s the smallest size the sensor…
Hello Emrehan,
Adding a fixed series inductor decreases the measurement range because only a portion of the combined inductance is the actual sensor. It can also have a similar impact on accuracy in the system. More information on using a series inductor…
Part Number: LDC1612 hi team:
would you help to provide the reference circuit for LDC1612 If the area of the coil is 20mm*60mm, how many turns, how many layers, and what is the line width?
customer need this case to detect the coins from inside banknotes…
Part Number: LDC1612
Hi there!
I have a problem with the LDC1612 that I would greatly appreciate some help understanding.
I am using an LDC1612 in continuous mode with hardware interrupts to inform my microcontroller of new conversions. I have two inductive…
Part Number: LDC1612 Hi team
I checked the collateral and found at 400kHz I2C interface the trb(readback time) is 0.688ms, but I'm using this device at 144kHz. Could you please let me know what's the trb at 144kHz? Also, is there an equation that allows…