Part Number: LDC1614-Q1 Hello,
My customer would like to know how to deal with the pins when not used. Would you please tell me about it except power and GND pins? I checked the datasheet, but it doesn't show the information.
Best Regards,
Yoshikazu…
Part Number: LDC1614-Q1 Hello,
My customer is wondering if the addresses of all the channels from ch0 - ch3 increment or decrement automatically without declaring stop condition. For example, if ch0 is configured, the other data from ch1 - ch3 can be…
Part Number: LDC5071-Q1 Other Parts Discussed in Thread: LDC1314 , LDC1614 Hi!
I need to make a rotary angle sensor
Now I am using a magnetic hall sensor for the first solution but I need another magnet-free solution
Can I use an inductive sensor to detect…
Part Number: LDC1614-Q1 Other Parts Discussed in Thread: LDC1614 Tool/software: WEBENCH® Design Tools Dear all,
We are developing a position sensor using LDC1614, one of the most strict specifications is the high accuracy level required, thus we are searching…
Other Parts Discussed in Thread: LDC3114-Q1 , LDC1614-Q1 How would you be able to add inductive sensing to an LCD assembly to read the force of a user's touch on a car center console/information display?
Other Parts Discussed in Thread: LDC1614 Dear all,
Are there EMS and EMI test results with sensing circuit?
I concern about influence of noise of this device and LC circuit.
Best regards,
Other Parts Discussed in Thread: LDC1614 , LDC3114 , STRIKE Greetings
First, my apologies for the long post but we have a few questions about LDC ESD that we would like clarification on.
So we will try to be as concise as possible.
Background
Application…
Hello Sagar,
The LDC0851 is not designed for automotive applications. You will need to use a device with the '-Q1' suffix like the LDC1312-Q1, LDC1314-Q1, and the LDC1614-Q1. I will note that these operate differently from the LDC0851 in that they need…
Part Number: LDC1614 Other Parts Discussed in Thread: LDC3114-Q1 , LDC3114 ,
Hello,
We use LDC1614 on our own board to detect the approach of metal on our coil.
To optimize the energy consumption, we would like to slow down the sample rate (62.5sps) when…
Hello Jim,
You can re-flash the EVM following these directions:
Q1: I have 'bricked' my LDC1312, LDC1314, LDC1612, or LDC1614 EVM during a failed firmware upload attempt. What can I do to restore functionality?
Best Regards,
Justin Beigel