Part Number: LDC2112 Hello TI team,
in the last days we got some troubles with our coil system at the emc tests.
We did get some fales press events in our button system.
I suspect we have already found a mistake. This concers about the routing of the…
Hi Poki,
My apologies for the delayed reply. As long as the INx trace is fully enclosed by the mechanical structure it should be okay to only shield one side. An application that has an exposed cable between the sensor and the LDC2112 would need shielding…
Part Number: LDC2112 Hi TI:
Our MCU use I2C connect all device including LDC2112
We have ship mode that will turn off all device power except LDC2112 since we will use LDC2112 to wake up system
So that we need at ship mode the LDC2112 still work norma…
Part Number: LDC2112 Hello Team,
we use the LDC2112 in one of our projects. Therefore, the LDC2112 is going to detect inductive buttons.
The detection works but we have an issue if we press button very slowly. In this case the LDC2112 did not detect a…
Part Number: LDC2112 Other Parts Discussed in Thread: LDC1001 , LDC0851 , LDC1614 Hi team,
Is LDC2112 able to measure rotation angle and vertical position like below?
If it's yes, my customer will considers to use LDC2112 instead of LDC1001 since power…
Part Number: LDC2112 Other Parts Discussed in Thread: LDC1612 , LDC1312 , I like the ability of the LDC2112 to operate in stand-alone mode without an external MCU. My application is automotive. From what I can see, the only automotive-qualified LDCs are…
Part Number: LDC2112 Hi Kristin
If the LED is placed on the surface of the LED FPC , and the target metal is pasted on the back. ITB FPC is a coil .
1. Does the LED FPC affect the mechanical response of the button?
2.The distance from MB component to…
Part Number: LDC2112 Hi Kristin
If LED is placed on the surface of the LED FPC and the target metal is paste behind. ITB FPC is a coil
I refer to the specification sona957a, and put ferrite on the back of ITB FPC.
There is no hole in the target metal…
Part Number: LDC2114EVM Other Parts Discussed in Thread: LDC2112 , FDC1004 , LDC2114 Greetings,
We are in the process of integrating a custom coil design based on the LDC2112 sensor IC. We have recently purchased a LDC2114EVM development board along with…