Part Number: LDC2114EVM Other Parts Discussed in Thread: LDC2114 , LDC1612 , LDC3114 Hi,
I am testing the LDC2114EVM with the Coil PCB "G" . Below is the configuration on the registers and the capacitor= 470pF .
The data streaming graph…
Part Number: LDC2114EVM Other Parts Discussed in Thread: LDC2114 Hi,
Sensing GUI is unable to detect the EVM. Currently using windows 10.
Kindly help!
Thanks
Part Number: LDC2114EVMLDC2114EVM connected via USB to PC. The sensing GUI is not able to detect the module. Using the sensing solutions GUI v1.10.0. Kindly suggest some solutions to connect the GUI.
Thank you
Part Number: LDC2114EVM Other Parts Discussed in Thread: LDC2114 Hello!
What are the lighting conditions for the LEDs on the LDC2114EVM CPU board? I think these are LEDs that indicate the target approach level (frequency increase level). What are the lighting…
Part Number: LDC2114EVM Other Parts Discussed in Thread: LDC2114 Hello, The LDC2114 can provide a 12-bit (2's complement) measurement, so I would like to know what the relationship between the actual frequency and this relative value data is. If the…
Part Number: LDC2114EVM Other Parts Discussed in Thread: LDC2114 Hi TI:
I want use external MCU(3V3 level) to porting with LDC2114 on EVM
EVM will power by J1 USB connector
Could I directly connect J4 signal to external MCU?
Or I need remove U6 MSP430 IC…
Part Number: LDC2114EVM Hello
This is Fang from GREE in Zhuhai city.
We refer to TI coil sample, to make a coil by myself.
Parameters are below. Only yellow infilling I make is ok ? Any advices can you provide ?
Thank you so much
BR
Part Number: LDC2114EVM Other Parts Discussed in Thread: LDC2114 Hello,
Been playing with the eval kit for that sensor a while now but can't achieve functionailty i am after.
Basically if i move the target into sensor range after its powered i can…
Part Number: LDC2114EVM Other Parts Discussed in Thread: LDCTOUCHCOMCOILEVM , LDC2114 Hi team,
my customer use LDC2114 EVM and LDCTOUCHCOMCOILEVM , and have questions. they touch the inductive coil, the EVM no any response and LED is off.
could you help check…
Part Number: LDC2114EVM Other Parts Discussed in Thread: LDC2114 Hello
This is Fang from GREE in Zhuhai city.
EVM211X and Coil sample are used, but I found COM pin and IN pin is connecting in schematic (Doc :SNOU146A-January 2017- Revised July 2017), as…