Part Number: LDC5071-Q1 Other Parts Discussed in Thread: TIDA-010961 Hello,
I plan to design a hollow-type inductive absolute position encoder. We require a resolution of 17bit or higher,+/-0.05 Absolute positioning accuracy or higher.
I compared…
Part Number: LDC5071-Q1 Tool/software: Hi expert,
There have some cases want to check with you about the OUTx pin state.
Case 1: When VDD or GND connection is open, what are the state of all OUTx pins? Hi-Z?
Case 2: When one of OUTx wire connection…
Part Number: LDC5071-Q1 Tool/software: Hello,
Could someone advise about ASIL level rating and its sensitivity to stray magnetic fields?! Does this product have ISO 11452-8 certificate for maximum magnetic fields it can afford?!
Regards,
Masood
Part Number: LDC5071-Q1 Tool/software: Hello,
We want to use LDC5071-Q1 for Steering wheel angle sensor.
Do you have any reference materials for coil design?
Part Number: LDC5071-Q1 Tool/software: Dear TI team, Recently, our team is developing a motor control platform using IPS sensor. However, we found that the angle we get from IPS (Sin/Cos) output is related to the metal object. In case the metal object…
Part Number: LDC5071-Q1 Tool/software: Most ASICs designed for metal target inductive sensors allow for connecting two chips to the same excitation coil. Each sensor can measure its own set of receive coils. For instance, one set can be configured for…
Part Number: LDC5071-Q1 Tool/software: Hello,
I am hoping to use the LDC5071-Q1 with a custom linear inductive sensor to give me absolute position of a linear slide.
I have been playing around with the LDC5072 Sensor Designer Tool and looking at the…
Part Number: LDC5071-Q1 Other Parts Discussed in Thread: LDC1314 , LDC1614 Hi!
I need to make a rotary angle sensor
Now I am using a magnetic hall sensor for the first solution but I need another magnet-free solution
Can I use an inductive sensor…
Part Number: DRV5055-Q1 Other Parts Discussed in Thread: LDC5071-Q1 , DRV5055 , TMAG5173-Q1 , TMAG5170-Q1 Tool/software: Hi Teams,
Can DRV5055-Q1 be installed with a side vertical axis like the 3D hall shown in the picture?
From the customer's perspective…
Part Number: LDC5072-Q1 Tool/software: Related to LDC5072-Q1: Can't startup. Goes to bootloop - Sensors forum - Sensors - TI E2E support forums
Just for clarification.
Maked PCB with Lexc = 1.87 uH, Rexc = 1.72 Ohm, Lin = 0.615 nH, Rin = 1.96 Ohm…