Part Number: LF347 Hi TI partners,
I want to use LF347 as in-phase amplifier, the schematic as below figure.
Single VCC:+12V (±5% Tol)
The input:2.5V(±0.25% Tol)
R1,R2,R3:10kohm,±0.1%Tol
…
Part Number: LM3290
Someone already asked this question but the answer was send directly to the person. Can anyone tell me the values?
question:
does anyone know who is the author of the below application note:
AN-301 Signal Conditioning for Sophisticated…
Part Number: LF347-N Other Parts Discussed in Thread: LF347 , LM324 , TL3474 We are replacing obsolete part MC34074P with the pin for pin TI part LF347N/NOPB in the attached circuit. Are there different operational amplifier formulas available to control…
Part Number: LF347 Other Parts Discussed in Thread: LF412 , , Hi
Our customers have questions about PCN.
This PCN is a change notification of FAB site.
What does the table below mean?
I understand that the device targeted for PCN is only LF412.
On…
Part Number: LF347 I have a board that uses many LF347M/NOPB devices but there is no stock at Digikey. There are many LF347DR devices. Can anyone tell what the difference is, or if there is a better replacement for the M/NOPB?
John
Part Number: LF347 Other Parts Discussed in Thread: TLV9002 , TLV9062 Hello,
I'm trying to use a LF347 op amp to amplify a 0-2.6VDC to a 0-3.2VDC and I'm running into an issue. I trying to drive to noninverting input to 0VDC but the lowest I can go…
Kiryl,
Clock output "wire" is just test point / informational. It doesn't do anything. Just measure the VF3 node with a oscilloscope , no load is needed because the output is a voltage signal.
LM358 would work but the edges would be much…
Part Number: TL082 Other Parts Discussed in Thread: LF347 , LF353-N , LF347-N , TL084
Hi, there.
1. I'd like to ask you information of TL082 open-loop gain and 3dB frequency.
I couldn't find any related figure in the datasheet.
2. I also wonder…
Richard,
I believe the capacitance will be the same as LF347-N (quad) two samples.
Cp is noninverting capacitance (to GND)
Cn is inverting capacitance (to GND)
Cd is input to input capacitance.
LF347LF347
Cp
3.3 pF
3.4 pF
Cn
3.5 pF
3.7 pF
…
OPA4172
OPA4132
OPA1654
LM837
LF347
Order now
Order now
Order now
Order now
Order now
Online datasheet
Online datasheet
Online datasheet
Online datasheet
Online datasheet
Datasheet
Datasheet
Datasheet
Datasheet
Datasheet
Tools & …