Part Number: BQ25619 Other Parts Discussed in Thread: BQ25618 , LM10506 Hi team,
We use BQ25619 with a portable product. It connects to a 18650 Li-Ion cell and the main system board with an MCU controlling the BQ25618 is powered by the PMID output. A LM10506…
Watanabe-san,
This issue has been tested and resolved on the LM10506 in this e2e thread: e2e.ti.com/.../661885
The LM10504 is very similar to the LM10506.
In this other thread, the SPI Write was also assumed to be valid, but in reality the SPI Write…
Bent, If a 3.2V LDO output will work in your system as the always-on rail (instead of the desired 3.3V), then I recommend you look at the LM10506. I see where your confusion is coming from now, as there are 3 conflicting statements in the LM10504 datasheet…
Hi, Doyel
Thank you for your continued support.
According to your answer about LM10504/06 internal pull up resistor,
LM10504/06 have an same internal pull up resistor (3MΩ typ.)
and you also answered before that it’s OK to keep the LM10504 RESET pin…