Part Number: LM1085 Other Parts Discussed in Thread: LM1086 Dear all! Trying to get a LDO LM1085 fixed 3.3V 3A (LM1085ISX3.3 NOPB, DDPAK/TO-263) running. But somehow I get a fixed output of 0.6V. I supply the part with a 6V (from voltage switching regulator…
Part Number: LM1085 Vout= 5V 3A
Vin=12V
Consider the TAB being soldered to a 1”sq copper pad on the top side of the PCB. The copper pad has via's connecting top layer copper pad with bottom layer copper pad. 4-layer PCB.
Two questions:
How long…
Part Number: LM1085 Hi experts,
My cusotmer select the ,but I did not find the thermal protection value in datasheet?
Do you have the specific value?
Thanks!
BR,
Gordon.
Part Number: LM1085 Hi, Support Team
We saw the LM1085 datasheet
about LM1085IS-3.3/NOPB for output cap of ESR range?
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: LM1085 Hi everyone,
I am looking for fully RoHs compliant alternatives for the parts listed below.
LM1085IS-12/NOPB
LM1085ISX-5.0/NOPB
LM2990SX-12/NOPB
Are there any better alternatives?
Kind regards,
Kavita
Part Number: LM1085 Hello E2E Experts,
Good day.
I want to 3.85V output. I adjust the resistors according to the formula in the datasheet but I got 4.18V output. Attached is the schematic.
I will feed the gsm module with this regulator I need 3.8-3.95V…
Part Number: LM1085 Hello Expert,
I want to clarify Case Temperature of Figure 5.
Is it Junction-to-case(top) temperature or Tc case temperature (surface temperature on the Case of Chip)?
Also, Could you please explain about "CASE TEMPERATURE AS LIMITED…
Part Number: LM1085 Hi Team,
i have a question on Lead finish/ Ball material of LM1085IS-ADJ
after running for several week, we found the color on Ball have changed: from white to yellow
does this normal? may i know the Lead finish/ Ball material on this…
Part Number: LM1085 I am using LDO (LM1085) in my design for conversion of 24V supply to 12V and it perfectly suits for the output current requirement.
I know that in order to ensure that the LDO works properly, I need to choose proper decoupling capacitors…
Part Number: LM1085
Hi Team,
We received inquiry from customer that our device LM1085 pin is not the same as indicated in the datasheet. For me to not miss anything, Ill copy the query below.
We have in our lab the LM1085 ADJUSTABLE in TO-220 and TO-263…