Part Number: LM1085
Hi Team,
We received inquiry from customer that our device LM1085 pin is not the same as indicated in the datasheet. For me to not miss anything, Ill copy the query below.
We have in our lab the LM1085 ADJUSTABLE in TO-220 and TO-263…
Part Number: LM1085 Hi TI,
I am using the fixed 3.3V output LM1085 LDO. When my design is powered on but not operating, the LDO has 1.1mA of current and about 2.4V output voltage. The input voltage is around 3.43V. When I begin operating the design my…
Part Number: LM1085 On page 19 of the LM1085 data sheet the bridge arrangement will cause damage itself and to everything up stream of it.
Please take note of the polarities of the rectifiers in Fig 25.
Part Number: LM1085 Hi support,
Could you please let me know 'Note4' of this mechanical data?
I couldn't find it.
Page 28 of the datasheet.
www.tij.co.jp/.../lm1085.pdf
This thread was taken off line. The oscillations were replicated on the bench but only when the minimum load was not being met for stability. Once the minimum load requirement was met, the oscillations stopped and the linear regulator was very stable.
…
Part Number: TPS7A4101 Other Parts Discussed in Thread: TPS7A44 , TPS7A30 , LM1085 Dear Team,
Do we have any LDO solution can meet the spec as below?
Vin=48
Vout/Iout= 28V(2A), 5V(30mA), -7.5(10mA), -3.4(10mA)
Many Thanks,
Jimmy
Part Number: LM1085 Other Parts Discussed in Thread: TPS54302 , LM337 We plan to use LM1085-ADJ to generate +7.5V and -7.5V from 12VDC input. Can we use this to generate neg output voltage? If so any ckt using LM1085-ADJ,
Attached a schematic for +7,5V…
Part Number: LM340 Other Parts Discussed in Thread: LM1085 i am searching for a lm340T-12 lt spice model, but cant find it on the site
Is this model available anywhere?
Part Number: LM1085 Tool/software: WEBENCH® Design Tools Hello,
I was attempting to export a PCB file of my Webench design for the LM1085, but it is not included in the export zip. I am only seeing the schematic & simulation files. It is also not available…