Part Number: LM1085 I know LM1085IS-ADJ/NOPB(DDPAK/TO-263) is RoHS Exempt device.
Do you have a plan to release RoHS corresponded device after RoHS exemption expiring ?
http://www.ti.com/lit/ml/szzq119f/szzq119f.pdf
Part Number: LM1085 Other Parts Discussed in Thread: TPS7A47 Hello,
I'm trying to convert 20V/5A SMPS power to 18~19V for my noise sensitive application. I couldn't find a good buck converter for my design.
I came across High-Current Low-Noise…
Part Number: LM1085 Dear all
I woud like to ask about output capacitor of LM1085.
After reviewing the LM1085 data sheet, the data sheet recommends that the output capacitor be 10uF tantalum or 50uF aluminum electrolytic. After confirming the following…
Part Number: LM1085 Datasheet C_out ESR recommendations for min allowed ESR (pg11, use Tantalum or Al Electrolytic)
conflicts with recommendation for low ESR (pg12, parallel ceramic capacitors indefinitely).
Please clarify.
Part Number: LM1085 Hi,
We are using LM1085ISX-3.3 voltage regulator for stepping down 24 V dc to 3.3 V dc .
Even for a load current of 200mA the IC is extremely heating. Is that due to the high drop out voltage (24 - 3.3 = 20.7 V) at the IC?
In the datasheet…
Part Number: LM1085 I tried to test this regulator. It was getting hot after some time. So I think there must be something that I am doing wrong. Please provide me with a circuit on which I can connect a load.
Thank you.
Part Number: LM1085 Hi Sir
May LM1085 can work in Vin 24V and Vout 20V 2A condition?
I check datasheet, it should be ok. but i can't run in webench.
if LM1085 can't be work. may we have other LDO can suggest?(customer need LDO because it will power…
Part Number: LM1085 Hi
I would like to know the ESD specification of the LM1085ISX-ADJ.
On DATASHEET, it seems that only the HBM value came out.
Can you provide HBM (Human Body Model), CDM (Charged Device Model)?