Part Number: LM1117 Hello, I have a query regarding the application of LM1117-3.3V regulator. The applications information suggests the use of Tantalum Bypass Capacitors. Can I instead use a ceramic bypass capacitor? And, what would be things I would…
Part Number: LM1117 Other Parts Discussed in Thread: LM317 The data sheet for this part says, "The LM1117 is a low dropout voltage regulator with a dropout of 1.2 V at 800 mA of load current."
We have an application where I'd like to get more current…
Part Number: LM1117 Hi Team, Our customer would like to ask for some clarifications on the thermal data seen on the datasheet of LM1117. Previous revision (particularly rev. M) of the datasheet shows a θJA of 136°C/W while rev. N and its latest revision…
Part Number: LM1117 Greetings,
This is a request from our customer from GILBARCO VEEDER ROOT INDIA.
Now customer is using LM1117MPX-3.3 in product ranges which is rated for 0-125degC.
he want to know the failure modes of this device when operated…
Part Number: LM1117 Hi LDO team
My customer is using LM1117-3.3 fixed output voltage version in their design.
I wondering to know are this device have requirement for minimum load current for output voltage regulation?
In datasheet I found such…
Part Number: LM1117 Team,
My customer is looking to add a 2nd source alternative to LM1117IMPX-3.3/NOPB on the current design. We would be second sourcing ourselves in this case. So, question is - do we have a pin compatible alternative to our device…
Part Number: LM1117 Hi Team,
Good day.
My customer is working with LM1117IDT-5.0 and wanted to clarification on the worst-case VOut performance with respect to temperature. Checking with section 7.6, page 8. of datasheet Vout is specified as 4.8 to…
Part Number: LM1117 Hello,
The ESR of the output capacitor should range between 0.3 Ω to 22 Ω.
Capacitor datasheet shows that ESR depends on frequency, so the minimum demand on ESR should base on which frequency ?
Part Number: LM1117 Hi team,
The typical current limit of LM1117 is 1.2A.
I would like to know what is the response after LM1117 detects current limit, shutdown the output and latch?
What is the delay time(response time) between LM1117 detects current…
Part Number: LM1117 Hi team TI
I bought some LM1117T-5.0 regulators this week directly from TI and i found out a old data sheet (August 2000) for LM1117 National Semiconductor that says the following:
"The ESR of the output capacitor should be less…