Part Number: LM117 Dear Sir,
During Incoming inspection of below part , following observations made:
1)On component body marking is faded in 13 qty , in as received condition.
2) Minor scratches observed in all components
L&T item code…
Part Number: LM117 Tool/software: Is this part LM117H/883 Available as stated below?
FINISH LEAD FINISH SHALL BE TIN/LEAD (Sn/Pb) WITH NO GREATER THAN 97% TIN AND GREATER THAN OR EQUAL TO 3% LEAD.
Part Number: LM117 Other Parts Discussed in Thread: LM317 Tool/software: Hello,
I am using the lm117 to generate a 2V rail, however, its output contains a lot of a.c. noise as shown below:
schematic is
I have added 220uF caps to both the…
Part Number: LM117HVQML-SP Other Parts Discussed in Thread: LM117 Hi all, I came across an old applications note 181 from National Semiconductor with details on the LM117 that go into more detail that the datasheet. I was wondering if TI had more information…
Part Number: LM117
Hello can you please provide what the "/883" denotes in the following part number LM117HVH/883? How is this different from the LM117HVH-QML?
Part Number: LM117QML-SP Other Parts Discussed in Thread: LM117 Hello,
I am simulating an LM117 configured for 5V output with a proprietary PSpice model and am observing a brief startup overshoot. The circuit is configured with several output capacitors…
Part Number: LM117HVQML-SP Other Parts Discussed in Thread: LM117 , We are able to find Total Ionizing Dose (TID) and Total Non-Ionizing Dose (TNID) test reports on the TI web site, but nothing on the Single Event Effect (SEE) characteristics. A National…
Part Number: LM117 Buenos días,
Lo dicho necesitaria un email de contacto para poderos dar de alta como proveedor en nuestros sistema que exije por la norma EN 9100 que tenemos que cumplir con un procedimiento que requiere de revision y firma de documentos…
Part Number: LM117 Tool/software:
can you recommend a TI replacement for the LM117H_NOPB please, ideally same three-pin can package and pin-to-pin compatable
Thank you
Part Number: LM117 Hello,
As LM117H/NOPB is Obsolete, I have choosen LM31AT/NOPB as an alternate.
But LM31AT has a operating temperature range (°C) of -40 to 125.
I am looking for an operating temperature range of -55 to 150 °C similar to LM117H…