Part Number: LM117HV Other Parts Discussed in Thread: LM117
Hello,
I am trying to use the LM117 as a current regulator using the following configuration (taken from the datasheet):
I was wondering if there is a reccomended way to evaluate the current…
Part Number: LM117HV
Hello,
Our customer did the sealing performance test about LM117H, and the tested results are not passed with both of the coarse leak detection and fine leak detection.
I am not familiar with the coarse/fine leak detection, so could…
Part Number: LM117HV HI dear I received several LM117HV that my agent bought those from TI . I recived and send my customer ,
but my customer return back them beacuse they have tow colore in pins ( they have gold cap and silver pins ) ilke soldering .
please…
Part Number: LM117HV Other Parts Discussed in Thread: LM117 Tool/software: WEBENCH® Design Tools HI My agent has bought several LM117HV from TI and send my customer ,
but my customer return back them beacuse they have tow colore in pins ilke soldering …
Part Number: LM117HV I am designing a circuit where the voltage is regulated from 15V to 9.15V. However, it overheats when there is no load for the regulator. And, even when I set the input close to the desired output input set at 13V. The regulator is…
Part Number: LM117HV Team,
We were using the 5962R07229 61 VZA (LM117HV) in a design, but that part is now obsolete so we’re looking at using the 5962R07229 62 VZA instead.
Do both parts use the same die?
If not, what are the differences?
Would you…
Part Number: LM117HV Hello,
We have a customer who is asking the following, we are not finding a clear answer in the datasheets:
"Have a question regarding Texas Instrument's LM117HVKSTL/883. What does the "STEEL (STL)" stand for in…
A review of a Worst Case Analysis revealed that an LM117HVHRLQMLV can have a transitory overvoltage condition applied where in Vin - Vout > 60 V. For a set 15V output, nominal Vin is 38 V, Iout is 22 mA. For a period of 10 microseconds, Vin might surge…