Part Number: LM137 I see the datasheet of LM137 and is not clear in the datasheet the difference between "Adjustment pin current charge" and "Adjustment pin current".
What is the external circuit to verify "Adjustment pin current charge" and "Adjustment…
Part Number: LM137 Hello,
We have a customer who is looking for plating information on this device.
There is a note in the datasheet which states Call TI, here in the Support Center, we are not finding the answer the customer is looking for.
From…
For TID, buy some time on a Cobalt-60 source and test it. This is not something that TI would do as part of their typical characterization. I have no idea what your application is, but for CMOS SEU is much more likely to be an issue than TID.
Or if…
Other Parts Discussed in Thread: LM137 In “minimum load current” you have the typ of 2.5mA but a maximum-minimum of 10mA (|Vin-Vout|=40V) in the LM137 Datasheet.
1. What's the point of saying "Typ 2.5mA? What for?
2. As Test Method what does it means…
Part Number: LM79L Other Parts Discussed in Thread: LM337 , LM337-N , LM137 Tool/software: Hi team,
Our customer is looking for negative output LDO that meet the following requirements:
Output Voltage: -0.5 V to -2.5 V (fixed output type)
Output…
Part Number: LM7800 Other Parts Discussed in Thread: LM137 , LM337 Tool/software: Hi TI,
I would like to build a basic Split Power Supply of +/_ 12V for Dual supply opamps working on breadboard.
I was researching and found there is a lot of bad designs…
Part Number: LM317 Other Parts Discussed in Thread: LM137 , LM337 The desired requirement of the requlator would give a 10V drop regardless of the input voltage. For an input voltage of 35 to 60V, the output would be 25 to 50V. It would track with the…
Part Number: LM337 Other Parts Discussed in Thread: LM137 Dear Sir/Madam,
I would like to find out the different between LM337I and LM137
1) what is the process technologies node, eg same type of die design for both part. is using bipolar process…
Part Number: LM337 Other Parts Discussed in Thread: TPS7A33 , LM137 Hello All,
For over 10 years I have been using LM337 and LM329DZ or BZ pair to have a low temperature coefficient regulator ( the circuit shown in every LM337 datasheet ). I need…