Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: LM1875 Other Parts Discussed in Thread: TINA-TI , , OPA564 Tool/software: TINA-TI or Spice Models Hello, i am trying to do a calibration and for this reason i have to use the sinus signal of a function generator. My generator can provide a signal…
Part Number: LM1875 Hi
What is the difference between different LM1875T part, for example LF02/LF03/LF05/LB05? I didn't find the difference in the datasheet.
BTW, the mark on the chip is "85ACT5UG3" "LM1875T", can you help to confirm if it is LF05…
Part Number: LM1875LM1875T/NOPB
Actually, we want to ask a question about LM1875 specification. Please support.
We try to design speaker amplifier with specification as below:
- Power Output : 20 W
- ± B Voltage : 25V
- Load : 4 Ω
Unfortunately…
Part Number: LM1875 Other Parts Discussed in Thread: TPA3136D2 , , TPA3118D2 I need a sine wave form coil driver chip. I want to generating magnetig field.
Coil 1mH / 3~4 Ohm (dc)
Frequency 10kHz, 15kHz or 18 kHz
Power Supply +/- 10V
Can I use chip for…
Part Number: LM1875 Dears,
We need to order LM1875 for our pilot run. Would you anyone can what's the difference between LM1875T/LF03 and LM1875T/NOPB. I cannot get related information from datasheet. thanks.
Part Number: LM1875 Have purchased few LM1875 op amps from a online spare parts dealer. The items looks to be little suspicious. Would like to confirm before using them. Can any one help identify if these ore genuine. Attaching herewith the photograph…
Part Number: LM1875 Hi Team,
We are confused about the orderable part number and the packages of LM1875T.
In its datasheet here
we can see it describes that it has a package type of KC0005A, which is a all-straight-leads package.
But we cannot see any…
Part Number: LM1875 Support Path: /Product/Development and troubleshooting/Find key information on a device/ Hello:
Why does the LM1875 typical THD vs. distortion curve (figure 3) have that odd shape, i.e., it rises with decreasing power, which implies…
Part Number: LM1875 Other Parts Discussed in Thread: TPA3128D2 Hi,
I am using LM1875 20W Audio Power Amplifier IC and made a circuit as given in the datasheet for Typical Applications For Single Supply Operation, I am giving the supply of 12VDC 1A and connected…
Part Number: LM675 Other Parts Discussed in Thread: LM1875 , Hi TI,
I was planning to use the LM675T to drive a low impedance inductive load. +/- 12V supplies, +/- 0.5A from DC-10kHz where my primary concern is very high signal fidelity: low THD and low…