Other Parts Discussed in Thread: LM20136 Hi,
Our customer plans to use LM20136 with inverting configuration. Then they need to know the gmps and gmea for it. Could you please disclose the information?
They are referring following application note to design…
Thanks,
You're right - that sounds like a lot of work.
I will look into using the LM20136 (to get to 6A at 1.1V).
It seems that if I need more current (say 12A), we cannot easily gang together switchers - and would need to find a bigger switcher.…
Eli,
If the 50mV or less output ripple voltage is important to you, you may want to look at another converter. TPS51315 uses output ripple voltage to directyly control switching so it requires a bit higher ripple voltage than some more standard parts…
Thank you for your support. However, we do not have enough time, please recommend us to reduce mis-operation. Solution is like below. 1. DC-DC Input : 12VDC We are using Flyback AC(98Vac to 242Vac) to DC Convertor circuit. Therefore, voltage 7VDC ~ 20VDC is…
Other Parts Discussed in Thread: TPS51219 Thank you for your support. However, we do not have enough time, please recommend us to reduce mis-operation. Solution is like below. 1. DC-DC Input : 12VDC We are using Flyback AC(98Vac to 242Vac) to DC Convertor…