Part Number: LM2104 Tool/software: Hello guys,
One of my customers is considering using LM2104 for step motor driving.
At this moment, They have the following question. Could you please give me your reply?
Q. Is it no problem to insert 100mohm resistor…
Part Number: LM2104 Other Parts Discussed in Thread: DRV8245-Q1 , DRV8873 ,
Hello Team, We want to design an H Bridge circuit to drive a DC Motor. The motor is a 12V DC motor with a maximum current of 2A. The inrush can be up to 10A but for only few…
Part Number: LM2104 Tool/software: The LM2104 has a fixed internal deadtime specified as 475 typical. There is no min or max deadtime or deadtime tolerance specified. What are the min and max deadtime for this part?
Part Number: UCC27710 Other Parts Discussed in Thread: LM2104 , Tool/software: Hi team,
Does TI have a p2p solution like EG2104S? thanks
https://file.elecfans.com/web2/M00/2B/DA/pYYBAGHWXKCAFqNjAAbGzoOiWts227.pdf?EG2104S_EG.pdf
Part Number: LM5104 Other Parts Discussed in Thread: LM2104 Tool/software: Hi,
how can i easily filter out single PWM input HB gate driver in the link ?
LM5104 is elder device, is any new version no-isolation HB gate driver IC which is single PWM…
Part Number: LM2105EVM Other Parts Discussed in Thread: LM5109B , , LM2104 , LM2105 Dear Specialists,
My customer is considering LM5109B and has a question.
I would be grateful if you could advise.
---
LM5109B doesn't have any evaluation board…
Part Number: UCC27301A-Q1 Other Parts Discussed in Thread: LM2104 , CSD19534KCS Tool/software: Hello -
I am looking for a recommended design or advice on a combination of half bridge driver and fets to drive a half bridge appiication at at least 20…
Hello,
I do not see the PWM input switching in the first scope shot. The output will not turn on until the PMW input starts switching.
Is the second screenshot after VIN was removed then reapplied?
This is also a very old part and I recommend…
Other Parts Discussed in Thread: UCC25800 Most applications including power delivery for industrial and automotive utilizing a half-bridge gate driver use the bootstrap diode and boot capacitor to generate the high side driver bias. This is the simplest…
Part Number: UCC27311A-Q1
Tool/software:
What are the considerations for using the high-side output of a half-bridge gate driver as a low-side gate driver?
When utilizing a half-bridge driver in a typical half-bridge configuration, an internal level…