Part Number: LM22675-Q1 Other Parts Discussed in Thread: LM22670-Q1 , , LM22675 , LM22670 Team,
I'm posting this on behalf of my customer. They would like to know if the LM22670-Q1 can be used as a replacement for the LM2267 5 -Q1? It looks like the…
Dear Frank De Stasi,
I have measured the current waveform, I don't think that it's cause hot by the saturation current, when short the output the peak current only 0.6A, you can reference the real waveform, and I don't konw why the frequency are not…
Part Number: LMZ14203H Other Parts Discussed in Thread: LM22670 , LMZ14203 , LMR38025-Q1 , LM70840 , LM76003-Q1 , LMR36015S Tool/software: I am using the LMZ14203H where the input is 24V - 36V and the output is 5V. this part has successfully passed our…
Part Number: PMP40988
Tool/software:
图腾柱pfc过零点畸变.pdf
Hello, I'd like to ask a few questions.
1. Single-phase totem pole PFC has zero-crossing distortion of inductance current, which can be eliminated by using soft start according to the document…
Hello Fhoude.
This is my RH850 board user manual.
r12ut0004ed0110-rh850f1km-s1.pdf
Connection between two boards is given below.
RH850 board TPS92682-069(EVM board --J10 connector is used)
Clock(P0_2) Clock (PIN no 12)
MOSI(P0_1) MOSI (PIN…
Hi,
I've attached the 2013 User's Guide for power products. Starting on page 53 you will find a selection of PWM controllers. many of these teh frequency can be varied according to external criteria.
As an example if you use a UC3842 it is a simple…
Gary,
Most any of our power controllers with dual output capability will provide the control. See attached document starting at page 50 with the dual output controllers on page 53 and 54 and choose what features you want.
Regards,
John