Other Parts Discussed in Thread: LM22672 Hi, We have an application using LM22672MRE-5.0 to convert VIN (12 - 24 VDC) to output 5 VDC. But this product also has the option to be powered by 5 VDC from USB or from a separate connector. So the question is: With…
Other Parts Discussed in Thread: LM22672
I've just received our prototype boards with the LM22672 5 V DC/DC. Problem is that the output voltage has oscillations when the load is increased. These oscillations are in the same frequency range as our…
Part Number: LM2672 Other Parts Discussed in Thread: LM22672 , TLVM13620 Hi to all,
I have a question regarding the LM2672MX-ADJ/NOPB.
As there are supply issues with this part and with all fixed voltage derivates!!
Is there a possible P2P replacement…
Other Parts Discussed in Thread: TPS54340 , LM22672 Hi folks,
I need to syncronize two cascade dc dc converter: first is TPS54340 (output voltage 12V), and second LM22672 (input 12V, output 3v3). I see in datasheet it's possibile to self syncronize two LM22672…
Other Parts Discussed in Thread: LM22672 It isn't clear from the documentation how much higher VIN needs to be over VOUT. I can only make inference from the duty-cycle calculation.
My application is VIN = 2x LION batteries in series, sum voltage of…
Other Parts Discussed in Thread: LM22672 , LM22670 , LM46002 Dear engineer:
Hello! I am a hardware engineer of Emerson, we selected LM22672 as our power chip, but I don't know how to choose input and output capacitor of LM22672, such as type, value of capacitors…
Other Parts Discussed in Thread: LM22672 Hi,
For our application we are utilizing small voltage regulator PCBs based on the LM22672 mounted onto a larger PCB (see attached picture). The input supply is 24VDC and the output voltage from the regulator is…
Other Parts Discussed in Thread: LM22672 I'm using a LM22672 to step down 24V to 5V. Occasionally (1 time in 200-300) the LM22672 will come up stuck in a limit mode at about 2.2 V with 140ns wide pulses. It will stay in this mode until power is cycled…
Other Parts Discussed in Thread: LM22680 , LM22672 Hi~
Out customer use LM22672/LM22680 device.
But Our customer have start-up problem.
* Condition :
- Vin : 10V, Vout : 7.1V
- Current : Nominal(Under 30mA : Non operating Motor), Active(1A, Operating Motor…