Other Parts Discussed in Thread: LM22672 Hello,
I would like to know the FIT value for LM22672 buck converter. Most TI parts have this data available in the web but not this one, maybe because it was a National product. FIT value is usually accompanied…
Other Parts Discussed in Thread: LM22672-Q1 , LM34919C-Q1 , LM2842-Q1 , TPS54140 , LM22672 I would like to confirm the operation with low dropout voltage and VIN<VOUT for LM22672-Q1, LM34919C-Q1 and LM2842-Q1.
For TPS54140(TPS57140), the problem occurs the…
Other Parts Discussed in Thread: LM22672 Hi
I have a question about EN pin voltage of LM22672 and other LM2267x.
The maximum voltage rating of EN pin is 6V as described in datasheet. But the voltage of this pin is 6.3V when this pin left open.
Is this…
Hello
It depends on what features and specs the customer is interested in.
I have attached a list of compatible devices that you may want to consider.
Thanks
Book1.xlsx
Part Number: LM2674 Other Parts Discussed in Thread: LM2671 , LM22675 , LM22672 We have several designs using the LM2674MX-5.0 and this part seems very difficult to source at the moment. I am looking for an alternative part pin to pin compatible which could…
Part Number: LM2576HV Other Parts Discussed in Thread: LMR36015 , LM22672 Hi,
I would like to do dc/dc buck conversion:
36-40V to 12V, @0.6-1.5A
12V to 3.3A, @ 0.2-1A (12V comes from the previous dc/dc)
I tried datasheet, evaluation board schematics and…
I am using a two LM22672MR-ADJ. One to generate a +16V
supply, the other to generate a -16V supply. Both converters are powered from
the same +24V supply rail. They are both synced from an external clock running
at 768Khz.
When I leave the enable…