Part Number: LM22676 Hello, I have a question regarding the value of the inductance Isat current for LM22676. If the max peak current limit of the LM22676 can be as high as 5.5A, shouldn't whatever inductance value you use still have the Isat of your inductor…
Part Number: LM22676 Hello, I would like to check with you about a p2p alternatives for the following PN :
LM22676TJ-ADJ/NOPB (the LM22676 parts family)
This is for future clients usage and currently it doesn’t matter if the p2p alternative is out of stock…
Part Number: LM22676 Hello, I use the LM22676 to bring a voltage from 24V to 5V. Recently, some of the LM22676 components have been giving me problems: as soon as they are connected to the 24V voltage, they burn out! Out of 100 components, this has happened…
Part Number: LM22676 What do the four characters "05ae" on the screen of this chip mean? Can we see information like production date from the silk screen.
Part Number: LM22676 Hi team,
My ctm use LM22676 as the buck dc/dc in their system, which is only dc/dc. 12 Vin and 3.3 V out, the processor is NXP RT1052, PHY 8081.We can't pass GBT 9254_ClassB EMI test.
the testing data \ sch and PCB file are as…
Part Number: LM22676 Hi,
I have a design that implemented on a board.
I use the LM22676 to convert 28V to 12V.
The board works but at the last year I have problem in some boards.
when I put a load of 1A the voltage drop down to 8.5V.
My question is what…