Other Parts Discussed in Thread: LM25019 , LM5019 hi Would it be possible to get the mathcad file or calculation tool including body plot of the lm25019 COT?
THANK YOU
Other Parts Discussed in Thread: LM25019 e2e,
We have a customer that needs an isolated output buck regulator capabile of Vin = 10V to 36V minimum and ouput current of 50mA. Figure 17 in the LM25019 data sheet provides an example schematic with Vin…
Part Number: LM5185 Other Parts Discussed in Thread: LM25019 , LM25017
Tool/software:
Hi all,
I need a DC-DC Isolation converter.
The Flybuck converter should be meet below given spec.
Input--24V
Output range -- 3.3V/40mA
If You have any…
Just noticed these devices you recommended is quite new. please suggest if LM25019 can support the same function? thanks.
http://www.ti.com.cn/product/cn/LM25019
Part Number: UCC28084 Other Parts Discussed in Thread: LM25019 , TL431 Hello,
This is my first time fully designing an isolated power supply. I am struggling with managing all of the design constraints: magnetics, power, slope compensation, isolated…
HI
suggest you used LM25019 as flybuck, and but frequency will be limited below 1Mhz.
for good regulation, suggest you add a LDO or zener at second for good regulation.
Thanks
Other Parts Discussed in Thread: LM25019 Hi,
I Need two +-18V supplies, one totally isolated one not. Found the LM25019, cheap chip, but sample Shows only 10V Output. The selection page give me that choice according my Input for +-18V.
Is this…
Other Parts Discussed in Thread: LM5017 , LM5018 , LM5019 , LM25017 , LM25019 , LM25018 Hello,
I am designing a data logger for 16 sensors, and I need to power sensors separately from isolated power supplies (each supply must be isolated from each other…