Part Number: LM25037 HI team,
Can you please share the LM25037 simlis model as customer is facing challenges with the transient model available online?
Thanks!
Harsh
Part Number: LM25037 Hi,
Can this part be configured for a PFC topology or can a part in this family be configured that way? If so how? Also could this be used to control GaN FET drivers (or an H bridge to implement soft switching)? If so how? Thanks! L…
Part Number: LM25037 Hi team,
I see reference online to a PMP7797 reference design that was a 6V-42V Input 12V/5A SEPIC for Automotive Applications. I don't see this on ti.com anymore, so I assume it was removed.
Was there a reason this design isn…
Part Number: LM25037 I designed electric schematic diagram than input voltage is 40~55V ,and output voltage is 24V ,schematic as figure below:
The problem is that output voltage is unstable , and LM25037's OUTA &OUTB PIN output the maximal duty cycle…
Part Number: LM25037EVAL Other Parts Discussed in Thread: LM25037 Hi guys,
I'm thinking about using the LM25037QMT to design a boost converter that would take a 12V input from my battery and convert it to a 24V output.
I want to use a topology of an…
Part Number: LM25037-Q1 Other Parts Discussed in Thread: LM25037 Do you have a calculation method for the working loss of this ti power chip? Please provide the relevant formula or algorithm, thank you!
Part Number: LM25037-Q1 Other Parts Discussed in Thread: PMP11186 Hi, Good day. Our customer has an inquiry about the PMP11186 which uses the LM25037-Q1. Kindly see below: I have been going through the PMP11186 Schematic which uses a push-pull topology…
Part Number: LM25037 Hi Team,
My customer plan to use LM25037 in open loop mode, below is their simulation circuit:
But customer found that there is no output on OUTB:
Would you help to share some help on:
1, Is the circuit is right or not?
2, Do you…