Part Number: LM25066 Hi Team,
If the voltage of OUT is higher than that of SENSE, and the voltage of SENSE is higher than that of the VIN, What will happen?
Regards, Hailiang
Part Number: LM25066 Dear Team,
Please help to confirm whether LM25066APSQ/NOPB and LM25066PSQ/NOPB can be replaced with each other, what is the difference? At present, the customer's project needs to import some substitute materials due to LM25066APSQ…
Part Number: LM25066 Dear Team,
Please look at the difference between the value read by LM25066 and the actual value, the difference between the two is about 1A. value read by LM25066;
Actual value:
By reading the register value root@sonic:/home…
Part Number: LM25066 Hello,
Taking a look at the reference schematic in the LM25066 datasheet I see there is a CIN on the VIN pin, but on the EVM I do not see this.
I would thing that you cannot use this for hotswap applications since there would be…
Part Number: LM25066 Other Parts Discussed in Thread: SN1402039 Hi Expert,
Customer found CML fault always happened on SN1402039 device,
The 7E register value was 82. I guess it meant bit1 and 7 (communication fault and invalid command) were set.
could…
Part Number: LM25066 Hi Team,
The customer is asking that what is the difference between LM25066PSQ/NOPB and LM25066IPSQX/NOPB ? LM25066PSQ/NOPB is also rated at industrial temp -40 to 125c, the same as Industrial grade. Thank you.
Best regards,
Mik…
Part Number: LM25066 I see the LM25066 contains registers. What type of memory is used to store those registers (ie SRAM, DRAM, EEPROM, Flash, etc.)? In particular, I am interested to know if these registers are volatile or non-volatile.