Part Number: LM25066A Hi Expert,
Please see the below picture then you can refer the register value on DEh (READ_AVG_IIN) which read from BMC.
The blue frame is CODE and the red frame is register value.
I think the mark A is the DEh register value right…
Part Number: LM25066A Other Parts Discussed in Thread: LM25066 , , LM25066I , LM25066IA Hello Expert, Our customer consider to replace to LM25066A from LM25066. Then, they have questions for these device as below. First, I confirmed datasheet from the point…
Part Number: LM25066A Other Parts Discussed in Thread: LM25066 , , LM25066I Hi team,
Customer now use LM25066A, due to shortage issue, they are consider move to LM25066.
While in LM25066A application, they didn't load any image to it; when switch to LM25066…
Part Number: LM25066A Other Parts Discussed in Thread: LM25066 Hi TI experts,
I used LM25066A for 12V hotswap design. We have one issue is that PGD goes low which trigger system shutdown (PGD low is monitored by FPGA and then it shut the board).
However…
Part Number: LM25066A Hi Team,
The customer wants to confirm whether LM25066A can use the program to shut down the chip? What do we need to do if we can?
Part Number: LM25066A Other Parts Discussed in Thread: LM25066 Hi TI experts,
I have LM25066A 12V hotswap design leveraged from existing project, where two 0.01uF caps are located on both side of Rsense.
Now let’s consider both C1015 and C1017 are stuffed…
Part Number: LM25066A Other Parts Discussed in Thread: LM25066 , CSD18536KTT Hi,
I'm testing the attached circuit.
1586.LM25066_Design_Calculator_REV_D.XLSX
Upon a series of cycling of power on/power off the circuit, the GATE driver ends up broken…
Part Number: LM25066A Other Parts Discussed in Thread: LM25066 Tool/software: Code Composer Studio Hi Guys,
Is there any Rs limitation for LM25066A input sense?
I found that the SPM_GUI couldn't show the right value if we used 0.15mohm Rs at P12V for…
Part Number: LM25066A Other Parts Discussed in Thread: LM25066 Hi,
Please check below questions, thanks.
1. I test LM25066 EVM, please refer to LM25066 Iin waveforms and the max current is 7.5A that is less than “IN OC FAULT” threshold, but it show …