Part Number: LM25066A Is the 16 to 28 uA Gate Pin source current range mostly dependent on part to part variation?
Figure 8 in the Typical Characteristics show that it's not dependent on temperature very much (at least for 5V-17V operation).
Part Number: LM25066A Other Parts Discussed in Thread: LM25066 Hi Praveen,
I hope all is well! I have a question regarding the LM25066A.
After reviewing the design calculator, it looks like my implementation will require two FETs instead of one FET. With…
Part Number: LM25066A Other Parts Discussed in Thread: TINA-TI , LM25066 Hi E2E,
Good day.
We have a customer looking for the un-encrypted model for LM25066A. The only available model is the encrypted one from PSpice on the device product page.
LM25066A…
Part Number: LM25066A Other Parts Discussed in Thread: LM25066 Hi Team:
it is known we will propose customer to use a clamped TVS to suppress the voltage energy when transient or hot wrap activity occurs, However, some Practical running results shows…
Part Number: LM25066A Other Parts Discussed in Thread: LM25066 , , TPS24770
Hi,
LM25066 has 25mV minimum current sensor threshold, for larger than 100A current application, the power loss on shunt resistor is too high.
Customer wants to add an amplifier…
Part Number: LM25066A Other Parts Discussed in Thread: LM25056 , LM25066 I have an application where I'd like to use the LM25066A without a hot-swap FET and only use the monitoring functionality.
Is this recommended by TI? If so, what should the connections…
Part Number: LM25066A Hi,
We issue the READ_VOUT command, and Rs=0.15mΩ, then how to get the real world Vout? I have read Table 41 and Table 42 in LM25066APSQE.pdf, but still confused. Under Table 42, there is a sentence:
For example, if a 5 mΩ sense…
Part Number: LM25066A Other Parts Discussed in Thread: LM25066
Situation is as following, the Overvoltage is set to 13,55V I increase input voltage to 13,6V, the output MOSFET is switched off. Input voltage goes back to 12,5V Now I am pulling down EN…
Part Number: LM25066A Hi Team:
There is an potential system risk if using 2 separated Hotswap LM25062 to produce P12VA and P12VB(PSU_P12V_VIN ---->P12VA&P12VB):
Since 2 large current Efuse share one common 12VIN, OV or Over current fault may be…
Part Number: LM25066A We are having trouble calculating the amperage passing thru the 2-milli-ohm RSENSE SHUNT resistor using the LM25066A 2016 Datasheet; the CL=GND. what is the proper equation to determine the current ?
thanks,