Part Number: LM25085A Other Parts Discussed in Thread: LM25085 , LM61495 , LM61460
I downloaded the PSPICE model from the LM25085A page for use in my own simulations, but it seems to be a model for the LM25085 instead since the reference voltage is…
Other Parts Discussed in Thread: LM25085A , LM25085 Hi. From Italy. I built this power supply with 30V input 12V output 3.5A output based on Webench software. (see diagram below). The result is that I have 17V at the output instead of 12V, both with no…
Part Number: LM25085 Hi,
Due to supply issue, customer plan to change from LM25085 to LM25085A. please kindly let me know if could P2P replacement without design changing. thanks.
Team, I found the mistake that was happening the problem was that the Chinese soldered the inverted component, inverted the component and got 2.4v is not the voltage I want more is just changing the resistor 6.04kohm to 3.74kohm I have the output of 3…
Part Number: LM5088 Other Parts Discussed in Thread: LM25085A , LM25085 ,
Hi,
I have used the WEBENCH tool to help me with the design of 4 power supplies. Following are the main features of them:
Vout1: +15V/4A (Input +24V);
Vout2: -15V/4A…
Hello,
I want to follow up on this post. Please let me know if you have any additional questions. If not, I would like to close this E2E post.
Thank you,
Katelyn
Hi,
Could you measure what is the FB voltage on LM25085A with and without the injection circuit with a digital multi meter?
Also, what happened if you changed C2 into 0.1 uF instead of 0.01uF
Thanks
-Arief
Part Number: LM25085A Tool/software: Webench Support Path: /Tools & software/Help me with an issue/WEBENCH Power and Analog Design Environment/Issue with WEBENCH Power Design/Power Designer/ Hi,
When running a webench design, webench came up with…
Part Number: LM25085A Hi
The customer considers DC motor drive system using LM25085A.
The requirement for LM25085A is as follows.
INPUT:17V-25.2V
OUTPUT : 16.2V/3A (8A peak)
EN function
4276.e2e.xlsx
It does not have motor driver,…
Part Number: LM25085A Hi
We plan to operate LM25085A with following requirement.
INPUT:17V-25V
OUTPUT:16V/3A (8A peak)
Enable
LM25085AMYEEVAL could not support for this requirement.
Could it be feasible to design custom board using…