Hi Matthew,
I have not seen an update on this thread for the last 15 days.
If the issue is solved it would be great to press the is solved button.
If there is still something open, just let me know with the new details.
Best regards,
Stefan
Hi Kevin,
the LM25118 would be able to handle that.
How to generate a negative output can be seen in this application report:
PMP20566 reference design | TI.com
When you say to generate -3.6V and -12V - are this two different designs which should use the…
Part Number: LM25118 Hi Team,
could you share how to induce equation (16) of LM25118 datasheet?
especially I'd like to know the purpose of VIN(MIN) in equation (16).
in SLVA535B, Peak inductor current describes as below and when I apply Dboost=1…
Hello Praveen,
Yes please, keep me update if this is improved. So far i can manage setting Tamb to 30ºC and add to the results the difference to the fina Tamb
Thank you for your support
Part Number: LM25118-Q1 Other Parts Discussed in Thread: LM25118 Hi,
I'm trying to simulate a buck-boost converter circuit that includes LM25118 in LTSpice with unencrypted lib file. It does not work properly and when i stop the simulation i get an error…
Part Number: LM25118 Hi everybody,
We use a LM25118 in buck-boost mode with a Vin 9.6V-22V and an output of 12V, 2.3A.
The initial design show an overshoot at the converter frequency. This overshoot is see on buck boost mode.
We add snubber on diodes…
Part Number: LM25118-Q1 Other Parts Discussed in Thread: LM25118 While performing simulations in Ansys HFSS using the Spice file of " LM25118Q1MH/NOPB" provided on your website, I'm running into the following error.
snvmaj9\lm25118_trans…
Part Number: LM25118 Hi,
We want to use the LM25118 for one of our products and for the same we made a schematic as attached.
We will be connect adapter on the input size and the adapter range is 15V to 24V , 5A and On the output side we need 15V,5A. …
Part Number: LM25118 Dear teams,
Whether LM25118 can implement following requirements?
Vin: 5-36V
Vout: 4 output with voltage 8V; Output current are 30/30/30/80mA, totally 170mA.
Customer is planning to achieve isolation at the output side with ratio…
Part Number: LM25118-Q1 Hi team, I check the pin-to-pin device LM25118Q1 and LM5118Q1, the only main differences are about the range of Vin and Vout, are there any other differences for customer need to pay attention to since they would like to use LM5118Q1…