Part Number: LM25118-Q1 Other Parts Discussed in Thread: LM25118 , TPS63060-EP Hi Team,
Could you help? I'm posting this in behalf of the customer.
I'm interested in the LM25118 pwm chip that TI offer's, specifically because it is catered to a buck…
Part Number: LM25118 In the datasheet , VOLL,VOHL,VOLH and VOHH were mentioned but those are corresponding to voltage across the pin to pin. kindly provide us the HO pin to ground and LO pin to ground (both in the high state as well as in the low state…
Hello LIN,
I expect that one of the recommendations in my first answer solved the issue. If this is not the case, please add another post below or if this thread is already locked, start a new thread.
Part Number: LM25118 Hello,
Our goal was to have a constant 12 Vdc output from a variable input of 12 Vdc or 24 Vdc, after some research we came across this component LM25118, and we found it suitable for our purpose.
We have designed a DC/DC converter…
Part Number: LM25118 I refer to a lm25118 adjustable output application circuit designed by datasheet, but it failed. I hope the engineer can point out the problem for me. Thank you. His problem is that he can only output a voltage of no more than 3.4V…
Part Number: LM25118 Hello! I designed buck-boost converter on LM25118 IC with parameters: Vin=16..24V, Vout=12...24V, Iout=3A.
If Vin>Vout, Iout=2A (Buck mode) converter works fine.
If Vin<=Vout, Iout=2A (Boost and Buck-Boost modes) converter only…
Part Number: LM25118 Hi. Help me please to understand why LM25118 isn't working in buck-boost mode. While Vin=24V, required Vout=12V / Iout=2.5A, LM25118 is working in buck mode correctly. But when Vin=10..12V, required Vout=12V / Iout=2.5A, I'm having…
Part Number: LM25118 Hi, I would like to use this or a similar suitable device to get an adjustable constant output current between 1A and 20 A out of 12V Vin. The current will be used in a chemical process. Could you give me some criteria or even a schematic…