Part Number: LM25137F-Q1 Hi Ti Expert,
For the entire LM(2)5137(F)-Q1 series, if we have Single Output with Dual Phase:
Can we short both nFAULT1/2 together?
Can we short both IMON1/2 pin together?
Could I just leave SYNCOUT pin as floating…
Part Number: LM25137F-Q1-EVM5D3 Other Parts Discussed in Thread: LM5137 , LM5137F-Q1-EVM12V Hi team,
What is the change for the EVM from independent output to interleaved output?
I made some changes in EVM but it does not work.
Regards,
Peter
It's in the product folder here: https://www.ti.com/product/LM5137F-Q1
Here is the link: https://www.ti.com/drr/opn/LM25137F-Q1-FS
(looks like the link is missing in the LM5137F product folder - I will get that resolved).
The key question is what is the input voltage, as this determines whether you use 40V, 60V or 80V FETs. If you use 40V FETs, then 20A/phase at 400kHz is relatively easy to do (see this EVM as an example: https://www.ti.com/tool/LM25137F-Q1-EVM5D3 ). …
Hi Ratheesh,
You can check the inductor vlaue using the quickstart file -- target 30-40% ripple current. Take a look at this EVM https://www.ti.com/tool/LM25137F-Q1-EVM5D3 , as it's setup for 5v and 3.3V out at 20A each, 440kHz, 1uH inductor.
In…
Part Number: LM5137F-Q1 Other Parts Discussed in Thread: LM5137-Q1
Tool/software:
Hi,
Regarding https://www.ti.com/product/LM5137-Q1 , https://www.ti.com/product/LM5137F-Q1
1) what are the differences from functional side of these two chips? …
Hi Nicole,
Yes that datasheet looks incomplete. For I would encourage you to used the user guide and the QuickStart calc until this issue is being resolved. 5428.LM5137-Q1_quickstart_calculator_revB6.xlsm and 7266.snvu891.pdf