Part Number: LM25141-Q1 We are planning to replace the existing 10 nF capacitor in the DITH pin using alternate part due to the component shortage. Can you share me what type of validation is possible to make sure the existing part and alternate part…
Part Number: LM25141
Hi,
I am designing a POL converter using the LM25141. I have 2 questions about it, and did not find the answer in the datasheet.
1) I would like to connect the EN pin to VCC or VDDA with a pull up resistor. Is the internal LDO …
Hi,
It appears that R5 was causing the issue.
I currently do not know why, but after removing it the RES pin works perfectly.
The current limit value has changed which is expected. Instead of using R5, I will need an inductor with a lower DCR for my required…
Part Number: LM25141-Q1 hi team,
What is the minimum deadband time in your manual? The manual gives only typical and maximum values. What does this deadband time look like with temperature? Is there a curve?
Part Number: LM25141-Q1 Other Parts Discussed in Thread: LM25141 , LM25149 , Hello sir,
Are there some reference circuits to enhance MOSFET drive ability? My customer wants to achieve 30A output current of LM25141. I used calculation tool to find the efficiency…
Part Number: LM25141-Q1 Other Parts Discussed in Thread: LM25141 Here are too states of LM25141, fix and adjustable feedback.
In fix mode, FB is connected to VDDA.
If i want to test the phase margin on fix mode, should i add and adjust the resistance on…
Part Number: LM25141-Q1 Other Parts Discussed in Thread: LM25141 , Hi team,
Do we have efficiency curve for LM25141-Q1 operating in 440k, 12V->3.3V, DEMB mode? Customer is evaluating power consumption with all LM25141 load disabled and found the real test…
Part Number: LM25141 Other Parts Discussed in Thread: LM5141 Hello!
I try to re-simulate an existing design using the LM25141RGER or LM25141QRGERQ1 to generate 5.20V @ 7A from 18V-38V with ~ 340kHz switching frequency.
If I select a switching frequency…