Part Number: LM25143-Q1 Hi team,
How to calculate or derive input impedance of a LM25143-Q1 circuit? It is used to design the input filter before the power supply.
In the below app note: The Middlebrook’s extra element theorem (paper [2]), explains…
Part Number: LM25143-Q1 Hello A sample PCB with Vout1: 12.5 V 30A, Vout2: 8V, and 12A output was manufactured using LM25143-Q1. However, the current output is not working properly, so please review the circuit diagram. Is it possible to request a circuit…
Part Number: LM25143-Q1 Hi,
The customer wants to use LM25143-Q1.
Spec 1 : Dual Output
Input Voltage : 21~27V
1Ch Output Voltage : 12.5V
1Ch Output Current : Max 30A ( Typ 25~27A )
2Ch Output Voltage : 12.5V
2Ch Output Current : Max 30A…
Part Number: LM25143-Q1 The followings are question for LM25143-Q1 from a customer.
1. データーシートの図9.9のようなインターリーブで 3.3V出力の仕様をWebenchで回路生成させるとVCCXはGND接続となります。 一方、図9.9(DS_P33)でのVCCXはVout(3.3V)に接続されています。この違いは何が原因ですか? If you generate a simulation bench circuit…
Part Number: LM25143-Q1 Hi team,
What is the Iq if configurate 25143 as two phase single output?
VOUT1=VOUT2=3.3V, DEMB=GND, MODE=VDDA
VOUT1 and VOUT2 are both enabled. I see in datasheet we only have Iq data in one enabled channel.
Thanks!
Part Number: LMR60420 Other Parts Discussed in Thread: LM25143 Tool/software: Which Buck Converter should i use to control Vin24V and Vout 0 to 18V by 800W?
Part Number: LM5143 Tool/software: Hi,
I had raised a question on this page: LM5143: External SYNC Support - Power management forum - Power management - TI E2E support forums . Unfortunately, I can't reply to that page anymore, as it is locked. Hence…
Part Number: LM5143 Other Parts Discussed in Thread: LM25143 Tool/software: Good afternoon, I use LM5143 to carry out a 24V to 12V dual-phase BUCK circuit, but it can't work, and the phenomenon is strange, the output is only 0.5V, and the SW has no waveform…
Part Number: LM5143 Other Parts Discussed in Thread: LM25143 Tool/software: Hi Team,
As title, does LM5143 recommended to use the condition?(4phase)
To minimized the MOSFET thermal issue, can we use 2MOSFETs in parallel?
If you have any recommendation…
Part Number: LM25148-Q1 Other Parts Discussed in Thread: LM25141 , LM25143 , LM5143 , LM25148 Tool/software: what does the gm=1200us mean ? why not uA/V ?
Is it the reaction time?